STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error/omission in RM0090: missing CC4NP bit definition

The CC4NP bit in the TIMx_CCER register should be listed in the reference manual in the section "17.4.9 TIM1 and TIM8 capture/compare enable register (TIMx_CCER)". Currently, only the CC1NP, CC2NP, and CC3NP bits are listed. The sections for the othe...

TDK by Super User
  • 1063 Views
  • 1 replies
  • 2 kudos

I am designing an PCB with an STM32H743 and IS42S16100H 1Mx16 SDRAM. I have two issues wiring up the SDRAM as detailed below.

The SDRAM has twelve address inputs A0-A11, where A11 is the bank select. In STM32CubeMX FMC section should I configure the SDRAM controller for 12 bit address and connect FMC_A0-A11 of the STM32H7 to the DRAM or configure for 11 bits and connect FMC...

SPape by Associate
  • 663 Views
  • 0 replies
  • 0 kudos

STM32F2 Emulated UART

I have implemented an emulated UART on STM32F2 using the sample program from STM32F4. The UART TX data output is correct. Until a HAL_Delay(100) is add. When added delay, the UART TX output appears corrupted as shown below. Why is the HAL_Delay affec...

0690X00000AqUYlQAN.png 0690X00000AqUYbQAN.png
JTan by Associate II
  • 2469 Views
  • 5 replies
  • 0 kudos

I am new to STM 32 MCU, it might be a basic issue I might be facing but couldn't find any solution in the documentations as well. When I am trying to connect STM 32 Nucleo and an IKS01A2 expansion board using a Unicleo GUI I am facing some problem

When I am trying to login to Unicleo GUI I am able connect to the communication port but the firmware description, version, expansion board name and library version in the login screen is showing unknown as I result , i suppose, am not being able to ...

0690X00000ArNWpQAN.png 0690X00000ArNWuQAN.png

I am working on H743. I have trouble getting ADC3 to work in continuous DMA transfer mode. I have ADC1 working fine but ADC3 wont work. Is there something wrong in my config?

After doing debugging i have found that the error code is set by DMA config function :HAL_StatusTypeDef HAL_DMA_Start_IT(DMA_HandleTypeDef *hdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t DataLength) { . . . . . else { /* Process...

sbstek by Associate
  • 1064 Views
  • 1 replies
  • 0 kudos

Exiting STOP mode

Hi,I am a new coder using the STM32L100RC discovery board. As such, my problem is quite simple I believe; I cannot exit Stop mode using an external trigger on the WakeUp Pin PA0. The code works as fallow: the LED on the PC9 pin light up, I enter STOP...

NBroc by Associate
  • 1292 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.