STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L081KZ,Dual-Boot,TIMER2 upgrade interrupt is valid in bank1, switch to bank2 is invalid! then switch to bank1 is valid???how

code 1: start:int main(void){ /* USER CODE BEGIN 1 */ LL_SYSCFG_SetRemapMemory(LL_SYSCFG_REMAP_FLASH); LL_SYSCFG_SetFlashBankMode(LL_SYSCFG_BANKMODE_BANK2);……}code 2:switch:void switchFlashBankToUpgrade(uint16_t BootBank){ HAL_FLASH_OB_Unlock();​ HAL...

Ewei.765 by Associate
  • 662 Views
  • 0 replies
  • 0 kudos

touch issue with STM32f303

Hi all,STM32F303 is as capability to sens touch which is surface touch principal . I am trying to get the values on STM studio but unfortunately i am not able to see any values on it. there always a flat line. I am posting my code can anyone tell me ...

ASaxe by Associate II
  • 760 Views
  • 0 replies
  • 0 kudos

How to relocate interrupt vector table in STM32L151RD?

Hello!I have written a simple application that reads a byte on USART (in an interrupt) and then sends the same byte back (simple USART echo). I have no problem running this application on various STM32 devices as long as the firmware is programmed at...

dzikos by Associate II
  • 2534 Views
  • 4 replies
  • 0 kudos

ADC3 Multichannel Scan Mode using DMA not working.

I tried doing line by line debugging to find out that Error code is being set by:HAL_StatusTypeDef HAL_DMA_Start_IT(DMA_HandleTypeDef *hdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t DataLength)To be specific, this line of the code:else   {...

sbstek by Associate
  • 861 Views
  • 0 replies
  • 0 kudos

SPI clock only giving 400mv

Hi I am trying spi master on the stm32h7 nucleo board, when I am measuring the spi clock it looks like it is only giving me 400mV max, can someone explain to me why and how to solve it? Thanks!

0690X00000ArQd0QAF.jpg 0690X00000ArQcvQAF.jpg

Resolved! DMA Flags not found (HAL Treiber)

Hello,I want to catch the half transfer and the full transfer flag from DMA controller but get an error and don't understand why.the compiler say first use in this function:'DMA_FLAG_HTIF5' undeclared (first use in this function)'DMA_FLAG_TCIF5' unde...

GIkar by Associate III
  • 2211 Views
  • 6 replies
  • 0 kudos

realize a dynamic display with stm32F401

hi,I have a projecte to realize with my stm , the idea of the system is :*sending images by smartphone to sd card which is connected to the stm board ,sending by using bluetooth or wifi communication.*display the list of images on lcd also connected ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.