STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

programming for STM32F302VB.

hi STM,i have STM32F303E-eval board which can me mapped to STM32F302VB mcu i/o lines.how to validate STM32F302VB source code using STM32F303E-eval board.please give inputs.regards,roushan kumar

Resolved! DMA cannot read SPI Data Register while Debuging in STM32F745

Dear All,I faced a problem and I would like to issue a note for other developers. If it is a hardware bug in microcontroller, it may also be helpful for ST developers to fix it for a later revision. Let me explain what I faced in detail. (While tryin...

0690X00000As8HhQAJ.png 0690X00000As8HXQAZ.png
TA1 by Senior
  • 1409 Views
  • 2 replies
  • 0 kudos

Supply external analog circuitry with AVDD?

So, I'm trying to integrate on a Test JIG a NUCLEO-144 with STM32F746ZG on board.It should be possible to draw some current since AVDD (CN10 pin1) is connected through a ferrite bead to the +3.3V (and in the user manual is written that the +3.3V can ...

Kepler by Associate
  • 2376 Views
  • 2 replies
  • 0 kudos

Polling or Interrupt better for CAN-FD reception

Hi,I have brought a new Nucleo-H743ZI kit. I wanted to receive data from 5 nodes using CAN-FD which transmits at the rate of 5mbps. which is the best method to use Polling or interrupt to receive the data over CAN-FD??Note: each node send 30 kilobyte...

VPras by Associate II
  • 1554 Views
  • 1 replies
  • 0 kudos

N-pulse waveform generation using STM32F767

Hi,I'm using STM32F767, Im trying to generate N-pulse waveform Generation but i couldn't achieve it.My TIMER configurations are static void MX_TIM2_Init(void){ /* USER CODE BEGIN TIM2_Init 0 */ /* USER CODE END TIM2_Init 0 */ TIM_ClockConfigTypeDef s...

VPras by Associate II
  • 2156 Views
  • 5 replies
  • 0 kudos

I2S Slave Receive issue losing sync

All,I am completely stuck with this problem I am facing where I2S receiving data seems to lose its sync with master. I am using STM32F412CG MC. When I power the MC, it receives data from master device, and plays back nicely. Next time when master sto...

ARash by Associate II
  • 1646 Views
  • 1 replies
  • 0 kudos

STM32F3 RTC Update issue

Hi All,I am trying to sync stm internal RTC by GSM. Now I am facing some issue. whenever I get the time from network I have to RESET the controller to get the network time.Do I have to reset the controller every time when ever I sync the RTC or there...

ASaxe by Associate II
  • 860 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.