STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SD lossless data storing from GPIO.

Hello,I am thinking to use an STM32H7 to write external data incoming from 16 GPIOs to an SD using the internal SD 4.1 Host controller. The data clock rate is 12 MHz.The STM32H742xI/G STM32H743xI/G DS (https://www.st.com/resource/en/datasheet/stm32h7...

simo zz by Senior II
  • 2230 Views
  • 5 replies
  • 0 kudos

STM32F373 SDADC HAL after Calibration, do I need to manual put an offset error value to final calculate with sdadc output value?

HiAs a title, after I call HAL_SDADC_CalibrationStartand HAL_SDADC_PollForCalibEventfollow Refference Manual page 240, calibration progress will store an offset error value in OFFSETx[11:0] fields. So do I need to read this value and put in the calc...

NNam.18 by Associate II
  • 1020 Views
  • 0 replies
  • 0 kudos

STM32072B-EVAL Display

Hi, Just purchased a STM32072B-EVAL board and loaded an example project on it. I cleared it from memory using ST visual programmer and now the LCD display is blank (i use to see the GUI). Did i accidentally erase the GUI? If so can I download it back...

canucktut by Associate II
  • 1473 Views
  • 3 replies
  • 0 kudos

STM32F100 RTC Wake From Standby is always 1 Second Late

Hello,I use STM32F100RBT. I want to enter STANDBY mode and exit every second.It works well, except for one issue: it always wakes up 1 second later.I run the following code, where I get the current time, print it and set an alarm for the next second ...

ISeed by Senior
  • 1768 Views
  • 1 replies
  • 0 kudos

Privilege for Interrupts

Hi, I want to deactivate all interrupts during a short period. I'm using __disable_irq();however, it says, that this can only be used in privilege mode. If I use this function my board crashes. I want to look up the privilege level, but the RM at pag...

SPI Master NSS always low in STM32F4

Posted on March 03, 2017 at 12:34Hi guys!I'm configuring the Nucleo 64 with the STM32F446RE to use SPI as a Master.The problem I'm having right now is that the NSS pin is always low. Clock and MOSI are perfect. What I would like is that the NSS is h...

0690X00000606TiQAI.png 0690X00000606TjQAI.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.