2019-11-13 6:38 AM
2019-11-18 2:36 AM
Dear Enrico,
It is possible to reprogram those GPIOs by default (upono reset) in Alternate Function, to any other state (input, output or another alternate function) and use them afterward. However you will obviously loose debug functionnality consequently and capacity to reprogram device using them directly.
A simple alternative would be then to connect under reset, assuming reset line can be connected from debug to MCU and reprogram the device after connecting under reset.
Best regards,
Antoine
2019-11-18 2:41 AM
You can programmatically remap early during startup, but not hard-coded when coming out of reset.
2019-11-18 4:26 AM
Not sure NRST is available
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.