STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PDR_ON effects to VBat?

Datasheet says Yes, but as we tested, RTC still runs (hold data after disconnected power), no matter what state of the pin is.Thanks for any suggesstion!

Dat Tran by Senior II
  • 861 Views
  • 1 replies
  • 0 kudos

Interfacing between SMT32F and ST L6206

Previously I've designed a motordriver based on an STM32F303 and an ST L6206 Dual Full Bridge driver. I've had some issues with the interfacing between the MCU and the bridge driver, because the MCU works on 3V3 and the bridge driver works on 5V. So ...

MAkke by Associate III
  • 1721 Views
  • 0 replies
  • 0 kudos

Problem with WiFi Connection in board B-L475E-IoT01A2

I have purchased a B-L475E-IoT01A2 board that WiFi connection works well in the company. But the problem is that when I take this board home and test it, it doesn't connect to Wifi. It should be noted that in both cases, I test this board with my mob...

Slh by Senior
  • 790 Views
  • 0 replies
  • 0 kudos

flash using USART for STM32F303E- eval

hi stm,i want to flash using USART. what is procedure.flashloader demonstrator is not working, it is getting hanged (win 7). but target is WIN XP.mcu board is need to connect with WIN-XP PC. how to achieve the target.

How to change output frequency of timer during run time

I am using stm32L073Rz I am using Tim2 channel 3 to generate different frequenciesAs per an example ,i configure timer 2 channel 3 in TIM_OCMODE_TOGGLE modewhen i generate code using cubemx i get the desired frequency using below code snippetbut i wa...

SA.17 by Associate III
  • 4088 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.