STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power consumption of the Nucleo 64 board : STM32L073ZR.

Hi everyone!I am trying to get the lowest power consumption from the STM32L073ZR in STOP Mode.I run my tests with the board powered from external source E5V (no USB connected).I have two Ampere-meters:one measure the current IDD of the microcontrolle...

SBour.9 by Associate II
  • 3581 Views
  • 5 replies
  • 0 kudos

Resolved! Need STM32 GPIO operate on 1.8v

Posted on August 03, 2017 at 20:26Hi, recently in a project I need the GPIOs on STM32 to operate on 1.8v logic level. By quickly looking through datasheets, it seems many of STM32 can do so, for example, to STM32F407VG, if provide 1.8v to VDD, it ru...

STM32H745XI power supply configurations

Hi Team,This IC STM32H745XI will support the following power supply configurations 1) Direct SMPS power supply which gives to the core domain 2) Direct LDO power supply which gives to the core domain  3) SMPS ->LDO-> Core domain(1.8v or 2.5v) 4) Exte...

SS_135 by Associate II
  • 820 Views
  • 0 replies
  • 0 kudos

How to Split the Flash memory in STM32f103c8t6

I want to know how to split the flash memory of the stm32f103c8t6 , The one part of memory is used to store the firmware & other part is used to store the settings & configuration through external user interface exe file. Please any one help in thes...

NO_ONE by Associate II
  • 1722 Views
  • 1 replies
  • 0 kudos

Continuous DMA from UART

Hello,This is for the STM32H7, but may be applicable to other STM32 chips.Is there a way to do a continuous DMA stream from a UART without requiring an expected size?I would like to be able to set up a receive buffer with DMA in circular mode, and ju...

ST User by Associate III
  • 3652 Views
  • 3 replies
  • 0 kudos

static_cast in C?

freqError = static_cast<int32_t>(readRegister(REG_FREQ_ERROR_MSB) & B111);C has no static_cast, so how can I convert the above code to C?(It 's C++, from Arduino)

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.