2019-10-09 3:44 PM
In my STM32H7 application I start a timer, stop it in an update interrupt handler (by setting ARR to 0), then when appropriate I set a new ARR value thus restarting the timer. This happens very frequently. During each such period I execute a number of compare interrupts. They happen say every 10 us. The timer prescaler is set so one timer count is one microsecond.
I observe some jitter between the timer start and the first compare event time. I suspect a reason for this is that the timer doesn't really start from 0 (even if I write 0 to CNT after restarting the timer, just in case). My guess is then, that the prescaler counter, that counts the actual 240 cycles before incrementing CNT, doesn't get cleared when I stop or restart the timer, or when I clear CNT.
Am I correct? And if so, is there a way to clear the prescaler counter so I'd be able to restart the timer from a REAL zero?
Solved! Go to Solution.
2019-10-10 8:30 AM
So I made an experiment on an 'F407 - enabled TIM2 and TIM4 clock in RCC; set TIM2 SMCR to SMS=0b111 exetrnal clock, TS=0b11 i.e. TRGI from TIM4; set ARR=3, PSC=3, set EGR.UG to force PSC to be active; set CR1.CEN=1; then in TIM4 in reset configuration, setting EGR.UG outputs one clock to TRGO, so I can then observe how after 4 clocks TIM2->CNT increments. This all in debugger, not a single line of code.
Using this setup, I observed, that
'twas fun :)
JW
2019-10-09 9:21 PM
Raise an update event by setting the EGR->UG bit. This will reset your timer and the prescaler.
Setting ARR to zero is an odd way to stop the timer. Consider clearing the CR1->CEN bit instead and setting to re-enable.
You're only going to get as good as the timer resolution, so 1-2 clock cycles at best. And if you're relying on the timing of an interrupt, that will add a few clocks jitter as well. But you should be able to do way better than 240 clock cycles.
2019-10-10 2:12 AM
Thanks, I'll probably do that.
Since I stop the timer inside an update event, then it's already been reset actually. So then it shouldn't introduce jitter when I stop it immediately at the handler beginning. Also, I played with CR1 |= TIM_CR1_OPM to enable one pulse mode, so the timer is automatically stopped at the update event. This turned out to be exactly what I was looking for, but then I realized I may need something else: to be able to chose if I want to stop the timer in the update event, or let it run. So I'll probably go with the CEN option. Originally I used zeroing ARR since I have to change it's value anyway, and the RM says it stops the timer, so why use two different commands when I could use one ;)
2019-10-10 8:30 AM
So I made an experiment on an 'F407 - enabled TIM2 and TIM4 clock in RCC; set TIM2 SMCR to SMS=0b111 exetrnal clock, TS=0b11 i.e. TRGI from TIM4; set ARR=3, PSC=3, set EGR.UG to force PSC to be active; set CR1.CEN=1; then in TIM4 in reset configuration, setting EGR.UG outputs one clock to TRGO, so I can then observe how after 4 clocks TIM2->CNT increments. This all in debugger, not a single line of code.
Using this setup, I observed, that
'twas fun :)
JW
2019-10-10 9:14 AM
That was a really great experiment! Thanks for sharing! It's great to know how this behaves under the hood.
2020-01-09 2:11 AM
TIMx->CNT = 0 wiil reset counter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.