2020-02-10 7:26 AM
I have an STM32L031F6 (custom) board. Using Jlink flashing tool we are trying to program the device but when we are trying to erase the board, we are getting the following error.
Erasing device (STM32L031F6)...
****** Error: Timeout while checking target RAM, RAMCode did not respond in time. (PC = 0xFFFFFFFF, CPSR = 0xFFFFFFFF, LR = 0x21000003)!
Failed to prepare for programming.
Failed to execute RAMCode for RAM check!
ERROR: Erase returned with error code -1.
2020-02-10 8:47 AM
Can you talk to or connect with the device using other tools/pods?
Are you correctly specifying the RAM location and size of the tools?
Do the same tools/settings work with other L031 boards?
Does it correctly identify the device. The log here is too short to gain much of any understanding of the problem.
If ST-LINK works properly, work with Segger directly for support.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.