STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cannot access memory of peripherals

Hello everyone,I am working with STM32H755ZI,, ARM GCC and J-Link GDB.Considering Reference Manual the H755ZI has following Memory Map (cutout):...0x40007C00 - 0x40007FFF UART8 0x40007800 - 0x40007BFF UART7 0x40007400 - 0x400077FF DAC10x40006C00 -...

MBos.1 by Associate II
  • 5360 Views
  • 11 replies
  • 0 kudos

What to use for HAL_SAI_Receive Size parameter?

Hi, I'm trying to work with the SAI HAL interface, i have set the black frame to 64 bits wide and the block slot size to 32B.When using the HAL_SAI_Receive() function, what does the length parameter represent?For my solution i am sending 2 32bit slot...

RBamf.1 by Associate III
  • 1205 Views
  • 1 replies
  • 0 kudos

STM32F74 vs STM32F7: Dual Bank Mode

I'm trying to get dual bank mode to work on an STM32F74. According to application manual AN4826 all STM32F7 series devices should be able to use dual bank mode. However, the reference manual for STM32F74 doesn't mention dual bank mode or Read-while-W...

NCentI by Associate
  • 765 Views
  • 0 replies
  • 1 kudos

Can you support 216MHz when using STM32F746 1.8V?

Hi all,​I am using STM32F746I want to check if it can be used at 216MHz when using at 1.8V.There is some confusion on the data sheet that makes it difficult to determine. (Attachments)Please help me ~Thank you,Best regards.​Gyosun.

sim20 by Associate II
  • 4406 Views
  • 6 replies
  • 0 kudos

Program JTAG-DP on STM32F102xx

We want to use the STM32F10x MCU as a JTAG dongle. Can we make use of the TDO, TDI and TMS on the chip or they are use solely for M3 debugging? Thanks.

aman.32 by Associate II
  • 1673 Views
  • 3 replies
  • 0 kudos

I am trying to process video signal from a linear CCD, is it possible to add two stop bits to the end of the digital output signal?

I am looking at options to replace my mostly obsolete design using an FPGA and old linear CCDs. I've already chosen a new linear CCD chip but I'm considering a handful of processing options. Our CCD alignment system currently uses 13 bits output to o...

AGipe.1 by Associate II
  • 2125 Views
  • 5 replies
  • 0 kudos

QSPI Interrupts not working with example projects

Hi,I'm using the STM32746 Discovery board and some example code - the "QSPI_ReadWrite_IT" example - but the QSPI interrupts are not working correctly. Specifically the Status match interrupt never fires and the example code gets stuck. I've ported ov...

DBurr by Senior
  • 740 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.