STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103C8Tx ADC count

Hello for my project I need 10 diffrent ADC's. I am planning to use STM32F103C8Tx for this project. In the dahasheet of it, "There are 2 ADC's with 16 external channels are available" information was given. So what I want to know is that, what is the...

GunkutA by Senior
  • 1666 Views
  • 4 replies
  • 0 kudos

UART RX FIFO not working

I can’t seem to get the FIFO to work on the RX side. TX works fine.Seems as if the FIFO isn't used. If I interrupt on the "RX not empty" event and read the data, it works fine. But as soon as I want to interrupt on any FIFO event, I never get the int...

ROost.1 by Associate
  • 1356 Views
  • 1 replies
  • 0 kudos

Data Collision between USART and SPI.

I my project I use UART 1 and 2 and SPI 1 and 2.When I send data via UART 1 using the function "HAL_UART_Transmit_IT (....)" and the second line in code I use the function "HAL_SPI_Transmit (....)" the data received from the UART 1 is incorrect, th...

DAvra by Associate II
  • 1457 Views
  • 2 replies
  • 0 kudos

External Interrupt in STM32F103C8T6

I am using STM32F103C8T6(Blue Pill) with STM32IDE.> I am trying to learn external Interrupt. So as a reference i am using 3 main thing. # Reference Manual # DataSheat # Cortex™-M3 Devices Generic User Guide> I wrote a code for this. I made changes...

Resolved! STM32F4-Not seeing an I2C signal

Hi, I'm using an STM32F429 MCU and trying to connect to a sensor through I2C. However, I measured both I2C pins with an oscilloscope and they were not showing any clock pulse or a signal. Here's my code for initiation:void MX_I2C1_Init(void) { hi...

JYang.4 by Associate
  • 1182 Views
  • 1 replies
  • 0 kudos

Let me know SPI communication in Register Level operation

Hi I am trying stm32f429zi discovery board for testing SPI communication​I've successed transmitting and receiving data on ADC chip​But I want know "How do these datas going so well?"​So I checked __HAL_SPI_TRANSMIT function​So I found that hspi->ins...

SKim.1761 by Associate III
  • 664 Views
  • 1 replies
  • 0 kudos

STM32G431 AN2606 discrepancy

The datasheet for the STM32G431 (DS12589 Rev 2) shows that the I2C3 peripheral is available on pins PC8 and PC9, but on page 206 of AN2606 Rev 42 it says that the bootloader is using PC6 and PC7 for I2C3. Since STM32CubeMX 5.5.0 agrees with the data...

galens by Associate II
  • 1134 Views
  • 1 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.