STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7. The I2C_FLAG_AF flag on I2C4 is always wrongly set.

I have an custom STM32H743 TQFP100 board. I use I2C 4, PB8, PB9 at 100kHz.The code is generated with CubeIDE.The I2C_FLAG_AF flag on I2C4 is always wrongly set and the transmission after adress is aborted.The device sends an acknowledge.Is this an bu...

FKuts.1 by Associate
  • 1281 Views
  • 0 replies
  • 0 kudos

Resolved! Semihosting - a lost cause?

I have a feeling i know the answer to this is "just give it up" but I figure before I do that, has anyone managed to get this Atollic thing working with semihosting and the J-Link? I ran up against Atollic's libnosys.lib defining _lseek and some othe...

n2wx by Senior
  • 1478 Views
  • 3 replies
  • 0 kudos

I appear to be having some issues with my DFSDM Manchester clock recovery. How do I set up the CKOUT for a 10MHz Manchester input? Do I need any clock connections or does it synchronize itself?

I am using the H7 and have a 10MHz sigma-delta ADC sending the Manchester signal. I do not have a clock going to the ADC because it generates its own.The internal DFSDM clock is set correctly, I think. I have a system clock of 96MHz and CKOUTDIV is s...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.