STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G431 documentation issues

The pdf file of the STM32G431 datasheet (DS12589 Rev 2) has an incorrect Title and Subject (it uses 474 instead of 431). My pdf viewer (evince) shows the following:Title: Datasheet - STM32G474xB STM32G474xC STM32G474xE - Arm® Cortex®-M4 32b MCU+FPU,...

galens by Associate II
  • 2019 Views
  • 4 replies
  • 1 kudos

Resolved! stm32f4 teraterm

Hello, I want to use teratern to send a string to my usart on stm32f4, but nothing is received. these are the settings of my teraterm

0690X00000D9AtpQAF.png 0690X00000D9AvRQAV.png 0690X00000D9AwZQAV.png 0690X00000D9AwFQAV.png
VYoun by Associate III
  • 5548 Views
  • 7 replies
  • 0 kudos

Hi, Is there a way to clear the bxCAN REC & TEC error counters without having to be connected to a fully functional CAN bus?

 I have tried resetting the bxCAN module, but that does not affect the counters.I have tried transmitting / receiving CAN messages in silent loopback mode, but that does not seem to affect the REC/TEC values.I am trying to clear the counters offline,...

MBrow.14 by Associate
  • 1061 Views
  • 0 replies
  • 0 kudos

Why does starting SPI1/DMA1ch2 cause ADC3/BDMAch0 to stop?

The HAL_ADC_ConvCpltCallback interrupts stop firing the moment I start SPI1:SET_BIT(hspi->Instance->CR1, SPI_CR1_CSTART);If I clear spi1's CR1 Start, I get the adc complete interrupts firing again.Since they use different peripherals, not sure how on...

EZamo.1 by Associate III
  • 1249 Views
  • 3 replies
  • 0 kudos

Non-continuous memory RAM on STM32H743II

Hi,I am developing an application running on STM32H743II MCU and I need to use all the 1Mbyte RAM.I tried to define a RAM_region for every SRAMx, this didn't work properly and not managed to build the project successfully.Another issue is that some ...

JKhal by Associate III
  • 1224 Views
  • 1 replies
  • 0 kudos

Problem in communication 2 slaves and 1 master using SPI.

hello everyone, I have a problem in communication 2 slaves and 1 master using SPI.master will send a code to activate one of the slaves and then the master will receive data from the slave, but sending the initial data is always wrong and only when t...

HAlau.1 by Associate II
  • 7326 Views
  • 19 replies
  • 0 kudos

Resolved! How do I properly exit from the fault handler?

I am currently using STM32F746. I am trying to exit from a MemManage fault handler back to the instruction which triggered the fault (I am trying something hacky that properly resolves the cause of the fault inside the handler so going back to the or...

KMaen by Associate III
  • 2468 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.