cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7. The I2C_FLAG_AF flag on I2C4 is always wrongly set.

FKuts.1
Associate

I have an custom STM32H743 TQFP100 board. I use I2C 4, PB8, PB9 at 100kHz.

The code is generated with CubeIDE.

The I2C_FLAG_AF flag on I2C4 is always wrongly set and the transmission after adress is aborted.

The device sends an acknowledge.

Is this an bug or my error?

On the Nucleo H743ZI2 I don't have these issues.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.