2020-02-18 12:26 AM
The TIM12 update interrupt is not occurred in TIM8_UP_TIM13_IRQHandler().
However it is occurred in TIM8_TRG_COM_TIM14_IRQHandler()
I configured TIM12 update interrupt as below;
//TIM4: master -> TIM12: slave
void MX_Test_TIM4_TIM12(void) {
NVIC_EnableIRQ(TIM8_UP_TIM13_IRQn);
__HAL_RCC_TIM12_CLK_ENABLE();
__HAL_RCC_TIM4_CLK_ENABLE();
TIM12->ARR = 16000; // slave timer period
// trigger selection TS=001 ITR1 = TIM2, slave mode SMS=0111 external clock mode 1
TIM12->SMCR = TIM_TS_ITR0 | TIM_SMCR_SMS_0 | TIM_SMCR_SMS_1 | TIM_SMCR_SMS_2;
TIM12->DIER = TIM_DIER_UIE; // interrupt on update event (timer overflow)
TIM12->CR1 = TIM_CR1_CEN; // enable timer 3
TIM4->PSC = 54; // prescaler preload
TIM4->EGR = TIM_EGR_UG; // update prescaler
TIM4->ARR = 250; // master timer period
TIM4->CR2 = TIM_TRGO_UPDATE; // master mode selection MMS=010 Update event
TIM4->CR1 = TIM_CR1_CEN; // enable timer 2
}
Let me know why TIM12 update interrupt is occurred in TIM8_TRG_COM_TIM14_IRQHandler()?
2020-02-18 2:57 AM
Why would be TIM12 interrupt associated with TIM8_UP_TIM13 ? Imo it should be associated with TIM8_BRK_TIM12 - see NVIC chapter in RM0410.
Check if the vector table in startup code / disassembly matches that in the RM.
JW
2020-02-18 11:08 PM
Thanks,
I misunderstand that TIM8_UP_TIM13_IRQn is an update interrupt from TIM8_IRQn to TIM13_IRQn like a EXTI9_5_IRQn (EXTI5_6_7_8_9).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.