2020-03-09 6:35 AM
Dear all, dear stm,
we ported our project from stm32F427 to stm32F765 because we needed more RAM.
After this we noticed that our code execution time has more than doubled.
We check all twice, ART, Cache, Interrupt, PLL, etc.
We tested also the Overdrive with no effect.
What could be the reason that the code execution from internal flash from stm32F7 is little more than two times slower than from stm32F4?
We are using Keil ARM Compiler V5.06 update 6.
Best regards
Dirk
Solved! Go to Solution.
2020-03-09 11:28 PM
Problem solved by Danish
Our Projektcode from stm32f4 start at 0x0800 0000, for stm32f7 ITCM bus it have to start at 0x0020 0000
Thanks to all and spezial to Danish
2020-03-09 7:02 AM
Zero optimization for the F7 project ?
The PLL does not startup, and the F7 runs on default HSI clockrate ?
2020-03-09 7:33 AM
Newer version of HAL, adding more bloat abstraction?
2020-03-09 8:32 AM
Where (in memory) is your program placed?
If (like stm32f4) you have it starting at 0x08000000 then accesses have to be via the AXI bus.
But if you place it starting 0x00200000 then accesses are via the ITCM bus, which I believe to be much faster, as well as not having to share bus time with data accesses.
Hope this helps,
Danish
2020-03-09 11:28 PM
Problem solved by Danish
Our Projektcode from stm32f4 start at 0x0800 0000, for stm32f7 ITCM bus it have to start at 0x0020 0000
Thanks to all and spezial to Danish
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.