2020-03-10 1:58 PM
I'm hoping this is a simple question. In the reference manual (RM0394 section 39.4.5), the tolerance of the LPUART receiver is specified in Table 204. For example, with BRR = 1024 and 9 bits/1 stop bit, the tolerance is given as 2.33%.
I've been assuming this means that all of the sources of baud rate error need to stack up so that the total is no more than +/- 2.33%. Is this understanding correct, as opposed to 2.33% total (+/- 1.165%)?
2020-03-10 4:23 PM
Yes, it means ±2.33%.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.