STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F030 Timer Delay -strange jitter

while (1) { GPIOA->BSRR = 0x0040; // PA6 Delay_us(100); GPIOA->BRR = 0x0040; // PA6 Delay_us(100); } //while(1)Hello ST after a lot programming with STM32F103 I startet with the STM32F030 and the STDPERIPH-Lib. Just an "easy example" of us...

0693W0000000APxQAM.jpg
werbung by Associate II
  • 5029 Views
  • 5 replies
  • 0 kudos

STM32F205 RTC can not periodical wakeup from Standby mode

Hi I am using STM32F205RCT6 to try periodical wakeup from standby mode. I choose RTC_WakeUpClock_RTCCLK_Div16 and set wakup counter 0x9000, that is about 18 Seconds @32768hz LSE. In main function,first print wakeup counter and RTC_CR, then every 1 ...

0693W000000TpfXQAS.jpg
Liu0155 by Associate II
  • 802 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H753 schematic and footprint

Hi, where can I find schematic and footprint for STM32H753 (or STM32H7 xx family) for Altium? In the STM32H7 and STM32H753 page I cant find nothing.Best regardsGMG

GMG by Associate III
  • 3437 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 triggering ADC with TIM6 TRGO

The ADC (ADC3 if that's relevant) provides for triggering by way of the TIM6 TRGO event. I have the ADC configured to convert with "ExternalTrigConv" pointing to ADC_EXTERNAL_TRIG_T6_TRGO, and the update event's rising edge. In no case am I able to g...

n2wx by Senior
  • 9076 Views
  • 25 replies
  • 1 kudos

STM32F427 SDIO Block Write with DMA not responding properly

I don't use libraries.My SD card interface is set up with an SDIO clock of 16.67 mhz using the 4-bit interface.My block write (SD command 24) works properly if I poll the data into the FIFO. The problem with that is the timing to push data into the F...

0690X000008wPbiQAE.png 0690X000008wPbsQAE.png 0690X000008wPbxQAE.png
Joe.H by Senior
  • 5435 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.