cancel
Showing results for 
Search instead for 
Did you mean: 

I have STEVAL-IDP005V1 and Nucleo64 boards. For the first time, STEVAL-IDP005V1 and Nucleo64 boards are Connected and programmed bin file and got output. But afterwords failed to reprogram STEVAL-IDP005V1 using Nucleo64 board.

KChin.7
Associate

Getting Following Error: "There is not enough space on NODE_F070RB. You need an additional 124 KB to copy these files."

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ETheu.1
Associate

Hi,

you'll need to connect the IDP005V1 over the M12 cable to a suitable power source.

In our case the from ST provided cable had the wrong wire-coloring. So it did not work just by connecting the blue wire to GND and the brown to VDD.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.