STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

cant get x or y values on XPT2046 over SPI on STM32F407VE

I just got https://stm32-base.org/boards/STM32F407VET6-STM32-F4VE-V2.0 which is my first foray into embeded. I also got https://www.waveshare.com/wiki/4inch_Resistive_Touch_LCD which is TFT with XPT2046 touch. I have the LCD setup with FSMC 16-bit bu...

3blake7 by Associate II
  • 2675 Views
  • 4 replies
  • 0 kudos

How do we define the frame buffer for emWin?

I found where we define the size of the screen but I could not find where the memory is allocated for the frame buffers. Also, emWin is running on 256k of RAM but the screen is 480x800. How do we define the bpp? Is it something that is defined in t...

MCons.2 by Associate II
  • 819 Views
  • 0 replies
  • 0 kudos

Implementation advice, DMA speed on UART and SDIO writing

I have two DMA streams running on my code for passing a CAN message buffer in memory to writing onto an SD card(tx/rx). I'm planning of using UART or SPI to retrieve a GPS unix-time stamp (module), my question is what should I be concerned for in usi...

WNguy.1 by Associate II
  • 815 Views
  • 0 replies
  • 0 kudos

STM32F303 UART Idle Line Detection Problem

Hi,i try to implement a idle line detection for my uart interface. I use this tutorial here: https://controllerstech.blogspot.com/2018/05/uart-using-dma-and-idle-line-detection.htmlIt is working on a STM32F103 (running example of the tutorial). So no...

STM32F769i-DISCO I/O pins

Dear All,I have a newbie question about the DISCO board.I need 3 or 4 I2C buses, but from the documentation I can find access only to one.Is it possible to access all other I/O pins of the MCU STM32F769NI on this board?I will highly appreciate all yo...

IgorKo by Associate II
  • 2573 Views
  • 4 replies
  • 0 kudos

Refresh STM32F469 Discovery Display

 Hi there.I am currently programming on an STM32F469 Discovery Board. Can you tell me what settings I have to make so that the display always updates automatically. So that all values ​​are always up to date?

HSchl.1 by Associate II
  • 779 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.