STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 N6 FSBL USART doesn't work

Hi, I have been trying to study how to use the N657X0 Nulceo board. When I tried to test the USART of the board with an FSBL project, there was no print on the serial monitor, and I could not find the reason. Could somebody check what the problem is ...

HANITALY by Associate III
  • 1283 Views
  • 1 replies
  • 0 kudos

Resolved! Question about STM32 H7 Series Function

[Inquiry Regarding Large-Scale Library Operation on STM32H7-Based System] MCU: STM32H7 Series (Planned) OS: FreeRTOS Memory Configuration: External SDRAM External Serial Flash (QSPI) Our company is planning to utilize large-scale libraries. We...

ishwang by Associate
  • 1203 Views
  • 1 replies
  • 0 kudos

SIL2/SIL3

Hi!May I ask the relevant safety experts from ST, I have now applied for the STEVAL-SILKT01 development board from ST Company and have signed the NDA. Are there any demo examples related to the STEVAL-SILKT01 development board? If so, could you provi...

HomeLand by Associate
  • 884 Views
  • 1 replies
  • 0 kudos

STM32G4 HRTIM burst mode enable / disable

In the reference manual for the G474, under HRTIM Burst mode control register (HRTIM_BMCR), bit 31 is the BMSTAT register; it gives the current operating status of the burst mode feature. But it states that writing this bit to zero causes early burst...

Jbin0101 by Associate III
  • 1730 Views
  • 1 replies
  • 0 kudos

SPI Slave on STM32G030F6 is not working

Hi, This is my first time here to write a post. I want to implement a system that connnects a STM32H723(master) and four STM32G030F6P6s(slave) via SPI communication. I connected  them and I check the SPI signals from STM32H723(NSS, SCK, MOSI). The Si...

JCho.3 by Associate III
  • 1808 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.