STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with STM32L475 Discovery kit IoT node power supply

Hello, I've just received the STM32L475 Discovery kit IoT node. I connected the board through USB cable to my laptop (the JP4 jumper is connected to 5V_ST_LINK) and the power supply LED (LD5) is blinking. Also the board is not visible from laptop (I ...

DMala.1 by Associate II
  • 2024 Views
  • 4 replies
  • 0 kudos

Resolved! Inverted polarity COMParator

Hello. I use STM32G474VET6.I want to use the comparator output as an external event for the timer. The output of the comparator (event) must be inverse (the POL bit is set in the COMP_CxCSR register). However, according to the logic of work, I see th...

ADedk.1 by Associate
  • 2950 Views
  • 2 replies
  • 0 kudos

ACCOUSTIC ECHO CANCELLATION: whodunnit ??

I have a speakerphone-ish application using STM32F405. Accoustic echo is a problem (mic picks up what the speaker barfs out). Prelim googling shows:Cube has add-on for speex AEC. But xiph (the guys who made the now-obsolete speex) themselves say...

Goof Ball by Associate III
  • 854 Views
  • 0 replies
  • 1 kudos

Hi, for several days now I have been trying to display a variable in "Snapshot acquisition mode" in STM Studio. The document CD00291015.pdf talks about this mode on page 21, talking about the "softTrace" subdirectory and the DataAcq.c and DataAcq.h files

Hi, for several days now I have been trying to display a variable in "Snapshot acquisition mode" in STM Studio. The document CD00291015.pdf talks about this mode on page 21, talking about the "softTrace" subdirectory and the DataAcq.c and DataAcq.h f...

Mbert.1 by Associate II
  • 1070 Views
  • 0 replies
  • 0 kudos

Program stucks on Timer2 Delay.

Hello,In my application there is an external interrupt configurations: RCC_ClocksTypeDef RCC_Clocks; RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); EXTI_InitTypeDef EXTI_InitStruct; NVIC_InitTypeDef NVIC_InitStruct; GPIO_EXTILineConfi...

AKara.3 by Associate
  • 1065 Views
  • 1 replies
  • 0 kudos

STM32G431 OPAMP not work?

Hi all,I'm using STM32G431KBU6, I've enabled the 2 opamps in cubemx, the settings for the opamps are: mode -- standalone power mode -- high speed user trimming -- disable I have 2 resistors and 2 caps to set the gain, low-pass cutoff freq and high-pa...

0693W000000VgyAQAS.png 0693W000000VgyKQAS.png
Jhon by Associate II
  • 1673 Views
  • 1 replies
  • 0 kudos

Read Out Protection Problem

Hi, I am using stm32f407vg. There is no read/write protection for sectors, there is only write protection option. So I had to enable read out protection, when I change protection level 0 to 1, code doesnt work. It's not working for even led blink cod...

0693W000000VdujQAC.png
kb24 by Senior
  • 2007 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.