2020-04-10 10:33 AM
I want to implement a CAN bus and I have the following boards:
I have seen that CAN interface is not avaliable in CubeMX for my nucleo board, so I have some questions:
Thank you!
2020-04-10 11:36 AM
Some chips do not support as it is cheaper when no license fee is paid and time on tester isn't wasted on exercising the IP.
Stuff on a shield, using third party ICs, via SPI, is not going to get code magically generated by CubeMX. Find example libraries for the shield and port into your project.
2020-04-10 3:02 PM
That CAN shield only has a CAN transceiver, it is intended to connect to a CAN controller such as the CAN interface available on many of the STM32 devices.
2020-04-10 5:03 PM
https://store.arduino.cc/usa/can-bus-shield-v2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.