2020-04-10 8:30 AM
Hello. I use STM32G474VET6.
I want to use the comparator output as an external event for the timer. The output of the comparator (event) must be inverse (the POL bit is set in the COMP_CxCSR register). However, according to the logic of work, I see that the inverter does not affect the polarity of the event. Are my assumptions true or am I doing something wrong?
Solved! Go to Solution.
2020-04-10 9:36 AM
I downloaded the version 3 manual. There are no more questions.
2020-04-10 9:36 AM
2020-04-10 2:58 PM
Thanks for coming back with the solution.
Please select your post as Best so that the thread is marked as solved.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.