STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 all GPIO pin capture with DMA and Timer

Hi, I am trying to capture all GPIO pin values when timer pin goes LOW. I cant understand which timer I need to choose? Which peripheral stands for GPIO port?How do I need to set Timer "Copy from" input source?I have STM32F091RC

JBond.1 by Senior II
  • 3316 Views
  • 7 replies
  • 0 kudos

MODBUS

Is it possible to implement modbus communication in STM32F401RE nucleo board ?If possible please explain the metho or please give me any tutorial

SUT by Associate II
  • 1018 Views
  • 1 replies
  • 0 kudos

STM32F767ZI USART abnormal Rx in interrupt mode

I do my code with CUBEMX 5.6.0 with en.STM32Cube_FW_F7_V1.16.0 & Atollic 9.2.0.My trouble : when i send a data by USART3 (using putty or the terminal in Atollic) even if i set that i want to recive 1 byte the HAL_UART_RxCpltCallback is fired two time...

Get hardware NSS mode for SPI with DMA in STM32 (F0/F4) working? Or alternatively manually start the according DMA channel (Low Level functions)

Hello,I'm trying to get a SPI communication in between two STM32 running with DMA. One is the STM32F051R8T7 (slave), the other ist the STM32F412ZET7 (master). There is nothing else on this SPI-bus. The best would be, if it runs with hardware controll...

0690X00000DYnRuQAL.png

Resolved! STM-STUDIO-STM32 - Snapshot acquisition mode

This STM software allows to monitor and modify the value of some variables in real-time using the SWD or JTAG connection in a non-intrusive way.In the documentation for the use of this software (https://www.st.com/resource/en/user_manual/cd00291015.p...

IBIS Model Check

Hi,I am using the STM32F413ZHJ6 in a design, BGA package. I have noticed some strange behaviour in the IBIS model of the part. When modelling the output of K11 and K12 (PD14 & PD15) the capacitance for the model is in the nF range. This is very large...

NMcGi.2 by Associate
  • 917 Views
  • 1 replies
  • 0 kudos

Resolved! Using SysTick causes reset?

UPDATE: The issue has been solved. The nBFB2 option bit had to be enabled.Hello, I am currently programming and STM32L152RE on a Nucleo development board. I am using SysTick as a .5s timer that ran a status LED. Everything was working up until recent...

SBona.2 by Associate II
  • 6053 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.