STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to make PWM one shot output?

Hello, I need to make software triggered one pulse output for 300 ms. The question is what is the best way to do this? I have found that PWM can work in one-pulse mode, but it looks like it requires external trigger to start, which is not an option f...

SAkhi.951 by Associate III
  • 2610 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F413zhj6 bga package, customer has noticed strange behaviour on the IBIS model. Capacitance on K11 and K12 is way to high in the nF?

STM32F413zhj6 bga package, customer has noticed strange behaviour on the IBIS model. When modelling output of K11 and K12 (PD14 ans PD15) the capacitance for the mdel is in the nF range. This is very large when compared to the other pins where they a...

ifosb.1 by Associate
  • 1319 Views
  • 2 replies
  • 0 kudos

Example software for STM32H747I-DISCO (STM32H747XI)

Hello, this is my first project with stm mcu and my development board is on the way. I would like to make a hobby wav player and I have found a rather good recipe to start with - AN3126 Application note "Audio and waveform generation using the DAC i...

ALevc.1 by Associate III
  • 2279 Views
  • 4 replies
  • 0 kudos

STM32F4 counce

Hi guys, i need to ensure there is no swtich bounce for my STM32F4.Expect use the HAL_Delay is that any way that i able to debounce it?I will include my code at following:tenButton_State fnenRead_Pushbutton(void){ tenButton_State enButton_State; enBu...

Cl.1 by Associate II
  • 721 Views
  • 0 replies
  • 0 kudos

STM32H743 SDMMC1 DMA Using

Hello. I am testing my own board with STM32H743.As the title suggests, DMA needs to be enabled.If don't using DMA, you can write SD card normally.If use DMA Enable, f_open will wait 30 seconds (just like the timeout setting) and will fail with an Err...

STM32L4 DSI camera

hellocan i use STM32F479 DSI host interface to connect with Raspberry Pi camera ( this camera has the same interface ).regards.Zakaria

ZTale.1 by Associate II
  • 722 Views
  • 0 replies
  • 0 kudos

Where can I find a table of STM32F745 DMA mappings to peripherals? In other words, what streams can I use for a peripheral?

I looked in corresponding reference manual (RM0385 rev 8) but all it appears to give is an "example" tables on page 226, which does not match what STM32CubeMX 5.2.0 says.I also could not find in the stm32f32F745xx datasheet (DocID027590 rev 4). The ...

JDwye.1 by Associate II
  • 2553 Views
  • 5 replies
  • 0 kudos

Resolved! I2C Slave transmit without HAL

I am writing a C++ I2C driver that would operate as a SLAVE device operating under interrupt and without CLOCK STRETCHING using STM32H732zi nucleo board My problem is that the first byte that I tried to transmit seems to always be 0xFF no matter what...

onio by Senior
  • 2433 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L011K4 ADC

Hello,where can I get more information on the STM32L011K4 ADC? Is there only one AD-core, wich is multiplexed to the different channels? How can I get the max. sampling rate?RegardsTobi

TK.1 by Associate
  • 1651 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.