STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to communicate with LCD2004a via I2C (Nucleo-F103RB)

Hell guys, i'm trying to communicate with LCD2004a with the I2C extender.i followed this guide https://www.youtube.com/watch?v=7mQppaEJjT4what i did:I generated project using CUBEMX to Keil uvisionconfigure I2C with those parameters: 100Khz CLK, slav...

Oyose.1 by Associate
  • 2243 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F746 SPI basic usage

Hi everybody! I've been struggling with this monster for a few days now. I'm trying to make it do some very basic (pun not intended) things and I have little hair left... But let's cut a (too) long story short: I'd like to send with the SPI a few byt...

luch by Associate III
  • 2585 Views
  • 3 replies
  • 1 kudos

Clarification of Entering, Leaving and Remaining in Sleep

Suppose that my system consists of 3 modulesmain... at the end of the while loop, I want the system to enter sleep mode, so at the end of the while, I put wfi(); or possibly I put DSB(); after that. Other examples replace wfi() with HAL_PWR_EnterSLEE...

DRobe.4 by Senior
  • 2867 Views
  • 5 replies
  • 0 kudos

Problem with using PLL and two SPI on STM32F103C8 bluepill

Hey there,I want to recieve two SPI signals sharing the same Enable Line, e.g. having exactly the same speed. I record them using the HAL_SPI_Receive_DMA function and count how many times SPI1 and SPI2 filled there respective Buffers. When using HSI ...

0693W000000WQcAQAW.png 0693W000000WQcFQAW.png
SWilk.1 by Associate II
  • 3191 Views
  • 7 replies
  • 0 kudos

Reflash target while connected with X-NUCLEO-LPM01A

Hello,I have a STM32L432 Nucleo32 and want to analyze its power consumption with the X-NUCLEO-LPM01A.I've read that there is the need to open connections to the STLink interface of the target.After that procedure, is there any possibility to reflash ...

Ab.1 by Associate
  • 698 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.