STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

which STM32 for an 8-channel DAC (f.x. PCM1690)

Hi =)I'm very new in the STM32 world - decided to upgrade from AVR to 32bit and I like the STM32 product series, documentation and community so here I am =) I would like to interface an 8 channel DAC with an STM32, for example a TI PCM1690.My questio...

SLasn.1 by Senior
  • 3328 Views
  • 4 replies
  • 0 kudos

Stack aligment in STM32f103, bit STKALIGN

HI. I'm trying to understand what is Stack aligment and what is it for. Cortex-M3 has a special bit STKALIGN in SCB->CCR register. Theoretically this bit is set to 1 in new revision of core, but when i look through debugger this bit is clear.I've rea...

sholojda by Associate III
  • 952 Views
  • 0 replies
  • 0 kudos

Resolved! GPIO data bus speed optimization/recommendation(s)

Greetings embed ProfessionalsRecently taken onto STM32 and getting along quite well so far! Regretting for not having done so earlier so plenty of catch up and "learning to do" (ps. mechanical engineering background here). Learning in particular; I'd...

Mecanix by Senior
  • 3629 Views
  • 9 replies
  • 0 kudos

STM32F411RE Unable to make UART work.

Hello guys.I've been trying to learn how to program STM32 MCU's using registers.This time, I've attempted to configure a basic UART programm in which I would like to send whatever I receive via UART back to the source. Basically an echo program.I'm i...

IRoja.1 by Associate
  • 2834 Views
  • 4 replies
  • 0 kudos

Resolved! stm32l552 bootstrap

Hi,I have a NUCLEO L552 and I would like to run a very simple program (just blinking a led).I have placed my vector table @ 0x08040000 as described by the data sheet. to program the flash I use the J-Link from Segger. What is strange, is that I canno...

STM32F446 ADC modes for analog watchdog

Hello,I'd like to use my STM32F446 in the following way:ADC 1&2 are connected to an analog sensorOnce the sensor connected to ADC 1 passes a certain voltage, start using DMA to transfer ADC 1&2 values to buffers.Once the transfer is complete, stop th...

RZige.1 by Associate
  • 2200 Views
  • 3 replies
  • 0 kudos

STM32L476RG USART not transmitting?

I'm trying to send exactly 8 bits of data, and check my results with tera terminal, however I'm not seeing anything come up. I noticed that on the block diagram for the STM32L476RG nucleo board, that the APB1 Bus is also connected to AHB1, but there ...

kfg4 by Associate
  • 1456 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.