STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 SPI rise time

Hello!I work with STM32F429 nucleo board.I try to connect it to CC1125 by SPI.The requirement of SCK rise time is less than 40ns.I tried different SPI channels and SCK pins.Typical SCK rise time of the board is about 50 ns.How can I improve it?

STolm.1 by Associate
  • 1651 Views
  • 2 replies
  • 0 kudos

STM32F4 cannot reset target

we use STM32F427IIH6,when we download the program the following error occurs:cannot reset target shutting dowm debug session;cannot access memory;internal command error;What causes the failure?see the attachment for further informationthank you!

cmeng.21 by Associate
  • 2617 Views
  • 1 replies
  • 0 kudos

Resolved! some misunderstanding on test board based on STM32F030RCT6

Hi. i have some problem when verifying the board composed of STM32F030RCT7 with Keil IDE (MDK ARM). I still don't know much about FW, so I ask a few stupid questions.​Problem 1. I am basically setting the project through STM32CubeMX. I checked that t...

DPark.2 by Associate II
  • 2282 Views
  • 5 replies
  • 0 kudos

RTC smooth digital calibration in STM32F4 with HSE

Hello,I am taking the liberty of writing to you for information on the calibration of the RTC.At present the RTC uses the HSE clock. The HSE clock is derived from a 25MHz quartz and then divided to be at 1MHz. This quartz has a tolerance of 20ppm.The...

Example to access DPM using FMC interface

Hello,https://www.st.com/en/embedded-software/i-cube-netx.html#overviewFrom this link, I am working for the PROFINET protocol using STM32F7 host and as given example it has worked for SPI interface.However, my requirement is to use FMC interface and ...

AP_040 by Senior
  • 2827 Views
  • 4 replies
  • 0 kudos

Rotary encoder turn detection

Hello!I want to use a simple rotary encoder with STM32F429.I programmed the TIM4 timer into 'ENCODERMODE_X4' mode.Is there a way for me to detect the rotation of the rotary knob by interrupt?I don't want to do periodically TIMx->CNT sampling if there...

PTiha by Senior
  • 2613 Views
  • 4 replies
  • 0 kudos

Debug uart via virtual com port (STM32F769I-DISCO)

Hello,Somehow I can't get debug uart via virtual port to work. I have followed several youtube videos and and studied user manual for my board that claims that "USART1 is directly available as a virtual COM port of the PC".The system debug is Serial ...

0693W000000WJlUQAW.png 0693W000000WJlfQAG.png 0693W000000WJq5QAG.png
ALevc.1 by Associate III
  • 2480 Views
  • 4 replies
  • 0 kudos

Connect a 8bit LCD to FSMC of STM32F103ZET6

I've been trying to connect a 8-bit LCD to FSMC of STM32F103ZET6. But it seems not working at all. Even the display ID could not be retrieved. So that is a complete failure!The LCD chip is ST7735S. This LCD works on other 8/16 bits mcu parallel inter...

CYuen.1 by Associate II
  • 1005 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.