2020-04-26 8:20 AM
Hi,
I have a NUCLEO L552 and I would like to run a very simple program (just blinking a led).
I have placed my vector table @ 0x08040000 as described by the data sheet. to program the flash I use the J-Link from Segger. What is strange, is that I cannot execute my program. Now, if I use Ozone from Segger, I can execute it, but when I power off-on the target, the program does not run anymore; again, Ozone can execute it. Probably, Ozone disables some protections ... any idea of what I have to add to my code to run in a non secure mode and make my code always executable?
Solved! Go to Solution.
2020-04-26 8:58 AM
Where does the datasheet or any other document mention that the vector table should be placed at 0x08040000 ?
It should be at 0x08000000 like on (almost) any other STM32, unless you have reprogrammed the boot address option bytes. Did you?
2020-04-26 8:58 AM
Where does the datasheet or any other document mention that the vector table should be placed at 0x08040000 ?
It should be at 0x08000000 like on (almost) any other STM32, unless you have reprogrammed the boot address option bytes. Did you?
2020-04-26 9:21 AM
Hi Berendi,
Correct! I was confused by some documentation.
Of course, the NS vector is placed @ 0x08040000. So, in NS mode, no need to operate with additional stuff.
Now it works!
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.