2020-04-25 3:32 AM
/* RTC init function */
static void MX_RTC_Init(void)
{
/* USER CODE BEGIN RTC_Init 0 */
/* USER CODE END RTC_Init 0 */
RTC_TimeTypeDef sTime;
RTC_DateTypeDef DateToUpdate;
/* USER CODE BEGIN RTC_Init 1 */
/* USER CODE END RTC_Init 1 */
/**Initialize RTC Only
*/
hrtc.Instance = RTC;
if(HAL_RTCEx_BKUPRead(&hrtc,RTC_BKP_DR2) != 0x32F2)
{
hrtc.Init.AsynchPrediv = RTC_AUTO_1_SECOND;
hrtc.Init.OutPut = RTC_OUTPUTSOURCE_ALARM;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initialize RTC and set the Time and Date
*/
sTime.Hours = 0x01;
sTime.Minutes = 0x20;
sTime.Seconds = 0x30;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
DateToUpdate.WeekDay = 0x07;
DateToUpdate.Month = 0x04;
DateToUpdate.Date = 0x25;
DateToUpdate.Year = 0x20;
if (HAL_RTC_SetDate(&hrtc, &DateToUpdate, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
HAL_PWR_EnableBkUpAccess();
HAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR2,0x32F2);
}
}
2020-04-26 1:12 PM
> I lose the date, but the time is correct
How are you verifying this? Seems the code you linked only sets the time/date if the backup register isn't 0x32F2. And if it is, your program does nothing at all.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.