2023-07-06 2:23 PM - edited 2023-07-07 10:34 AM
Hi!
I am using STMCube IDE and a STM32G030F6
I am trying to implement a code that writes variables to the flash. And I was able to make it work, with some limitations...
THIS CODE WORKS
union
{
uint8_t regs[6];
uint64_t data;
} mem;
uint64_t *my_pointer;
my_pointer = (uint64_t *)0x08007000; // base address of page 14
if(*my_pointer == 0xFFFFFFFFFFFFFFFF) // if the memory is blank
{
HAL_FLASH_Unlock();
mem.regs[0] = 25;
mem.regs[1] = 50;
mem.regs[2] = 75;
mem.regs[3] = 100;
mem.regs[4] = 1;
mem.regs[5] = 0;
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x08007000, mem.data);
HAL_FLASH_Lock();
}
I run this code in the initialization of the board, the first time the program runs it will enter the if...
Instead of using
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD...I'd like to use:
HAL_FLASH_Program(FLASH_TYPEPROGRAM_FAST...
But i am not able to make it work... it crashes all the time in the function:
static void FLASH_Program_Fast(uint32_t Address, uint32_t DataAddress);
What is the best way to write a series of variables in the flash? I plan to write more than 20 uint16_t...
2024-04-15 6:40 AM
Same here. The Flash_Program_Fast keeps crashing.
2024-12-24 1:02 PM
Anyone at ST that has just a little interest in helping its customers?
2025-05-28 5:22 AM
I have encountered the same issue, the FLASH_TYPEPROGRAM_FAST method crashes the micro and even aborts the debugging session.
A workaround has been to wrap FLASH_TYPEPROGRAM_DOUBLEWORD in a function that behaves (takes in the same parameters) as FLASH_TYPEPROGRAM_FAST, which then executes as expected and without an issue.
2025-05-28 6:20 AM
Would guess the issue here is that code has not been placed properly in RAM leading to unacceptable delays during fast programming. The __RAM_FUNC macro needs some help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.