STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F105 flash programming through CAN

I have an application where I must be able to update the code remotely through the CAN2 link and the embedded bootloader. This worked fine using the mass erase function, but now I need to erase sectors individually. The ap note AN3154 poorly describe...

JBizo.1 by Associate
  • 1953 Views
  • 3 replies
  • 0 kudos

Bare metal STM32F767 PCB design

Hello This is my first time using STM32 MCU on my own PCB. I know that I have to take many things into consideration. Please help me if I am missing somethingI have wired up all VDD/VSS/VDDA/VSSA/VUSB with bypass caps as close as I couldI have used e...

hashtala by Associate II
  • 2164 Views
  • 6 replies
  • 0 kudos

Resolved! ADC power circuit

Hello, I am developing a circuit using STM32L4R9AI, VDD = 1.8v, VDDA&VREF+ = 3.13v, according to ST hardware design manual (I attached) for a better power filtration there should be bead between VDD and VDDA, will that create a problem given the volt...

STm32L496 IAP and BLE

Hi !I've been trying to update my STM32L496 firmware over BLE.Our bootloader use Ymodem to transfer files (as it's explained in the Application note). I have connected the UART of my BLE chip with the UART of the STM32). I can send the file (only fro...

FGuil by Associate
  • 1484 Views
  • 1 replies
  • 1 kudos

Resolved! ADC overrun error. Multiple DMA usage.

Hi,I am using a NUCLEO F334 development board.I am using the ADC with the DMA. I developed that feature and tested and everything looked alright. I have been developing some more over that and I see that after startup the values are correct but after...

0693W000000WxBRQA0.png 0693W000000WxBHQA0.png
mur by Associate III
  • 9963 Views
  • 10 replies
  • 0 kudos

Ethernet STM32H7 DMA

Hi everybody,Currently we have a weird thing with Ethernet on STM32H7.Everything work fine if disable cache globally.When enable cache, work fine. We can send/receive few hundreds MB or keep ping /t from PC few days, no error. So we believe we config...

Dat Tran by Senior II
  • 1871 Views
  • 3 replies
  • 0 kudos

MAY i use Interrupt handler multiple times ?

In the follwoing code i would like to use same interrupt multiple times in order to blink the 4 leds different time. i am storing the data in unint8_t ABB, i expect that each time i press the button the value in ABB is incremented but practically n...

ALE1 by Associate II
  • 2733 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L052K8 custom board does not run while the same board for STM32F051K8 works (same pinout and peripherals on the PCB)

Updated Question:I have a custom PCB board with L052K8 and F051K8 with the same peripherals and correct hardware design for each (F051K8 has a VSSA for the ADC and different bypass cap), but only the L051K8 is able to program its firmware and reset c...

JLee.161 by Associate III
  • 3665 Views
  • 8 replies
  • 0 kudos

How to change the frequency of the PWM using potentiometer

Hello guys good day to you. May I ask you if you can share your experience on changing the frequency of a PWM using a pot. I am using a small board with the STM32F103C8 MCU. I've set TIM2 _CH1 of PA0 as output. I connected a potentiometer to PA...

RSy.1 by Associate III
  • 2765 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.