STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to get PWM from lidar sensor?

Hi everyone, i'm quite new with the stm. Currently im using the stm32f411 discoveryboard and trying to get the pulse width in order to measure range, i did try to search for solution and find out about input capture method but the code is on sw4stm32...

ĐNguy.1 by Associate
  • 2043 Views
  • 2 replies
  • 0 kudos

reason H745 not booting

Hi,I have a custom board with an STM32H745 which doesn't boot / I can't connect to.I've noticed that three of the gnd pins are not connected K15, L15, M15, would this cause the problem?The design is using an external 1.2V supply which is fine. 3.3V i...

SHanl.1 by Associate
  • 1432 Views
  • 2 replies
  • 0 kudos

Simultaneous use of two FDCANs of STM32H743

I am developing a device that simultaneously logs two CAN lines using the STM32H743.I saw "Wrong data may be read from Message RAM by the CPU when using two FDCANs" in STM32H743 Errata document.I need a detailed explanation of the above Errata.I am t...

SKim.2344 by Associate II
  • 1454 Views
  • 1 replies
  • 0 kudos

Resolved! What is the mining of #define SHUT_DOWN_TIME_OUT 20000UL?

HelloI'm using the "en.fp-sns-allmems2", which send data from sensor with a ultra-low power consumption. I'm traying to increase the time in which the sensor is in shut down mode.I think that I've to change the value of the variable  SHUT_DOWN_TIME_O...

NMart.1 by Associate III
  • 2392 Views
  • 4 replies
  • 0 kudos

DMA interupt

I know that DMA interrupt don't need rising/falling edge trigger because DMA interrupt is an internal signal.Except this result is that any additional result why DMA interrupt don't need rising/ falling edge trigger?

Cl.1 by Associate II
  • 822 Views
  • 0 replies
  • 0 kudos

Multiple read from Peripheral to Memory using DMA

Dear Experts,Can I configure the DMA2 to do say 3 repeats read on GPIOx_IDR by a single DMA request? I do not want to have array of bytes instead I would like to write into a single variable and overriding it with the latest value.I have set the MINC...

ADC whit DMA. stm32f0

Hi every one.I want to read the value of a potentiometer connected to the pinA1, and if the read value is more than 2000, one of the LEDs, otherwise the second LED, will be on.Can anybody please help me? what is wrong with my code? I don't have too m...

Nmo.1 by Associate III
  • 2466 Views
  • 5 replies
  • 1 kudos

STM32f4 Timer1 counting pulses

Hello all, I want to count pulses with TIMER 1, because he has the fastest counting frequency. I was able to count pulses with TIMER 2 but something in my code is missing to make it work for Timer 1: (I also checked the reference manual ...)Maybe som...

MKell.2 by Associate II
  • 3964 Views
  • 8 replies
  • 0 kudos

Resolved! STOP2 mode scrambles stack on STM32L4R9

I'm really struggling with this problem. This is my first time trying to do anything low power, so please forgive any noob mistakes. All I'm trying to do is get the hang of a simple low power program so I can apply it to a larger one. My code is here...

CBald by Associate III
  • 2429 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.