2020-05-13 7:16 PM
Hello guys good day to you. May I ask you if you can share your experience on changing the frequency of a PWM using a pot. I am using a small board with the STM32F103C8 MCU.
I've set TIM2 _CH1 of PA0 as output. I connected a potentiometer to PA2 (ADC1_IN2 ) to vary the frequency. I am using CubeMX to configure the MCU. Here are the other details:
MCU clock set to 48MHz
ADC clock set to 12MHz
TIM2 prescale to 47
TIM2 ARR set to 0 (I am thinking of modifying the htim period line to vary the frequency)
I used the HAL_ADC_ConvCpltCallback to enable the ADC.
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef * hadc)
{
htim2.Init.Period = ADValue/4; //I was thinking I could vary the frequency this way
TIM2 -> CCR1 = (ADValue/8); //Set duty cycle to 50%
}
However I do not see the TIM2_CH1 having output at all. Can you tell me what is wrong and how to correct this? Thank you for your time.
2020-05-13 7:22 PM
> TIM2 ARR set to 0
Your timer will not run with ARR=0. See the reference manual.
> htim2.Init.Period = ADValue/4;
This doesn't do anything but change a value in memory. It doesn't actually modify the timer register (which is done in HAL_TIM_Base_Init). You probably want
TIM2->ARR = ADValue / 4;
2020-05-13 8:14 PM
Thank you Sir I will try this code.
2020-05-13 9:10 PM
I tried this code:
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
TIM2 -> ARR = ((ADValue1[0])/4); //vary the frequency
TIM2 -> CCR1 = ((ADValue1[0])/4)/2; //Set duty cycle to 50%
}
It is working but I noticed the LED output is jittery. I am expecting for a smooth transition but the waveform/output is not stable.
2020-05-13 9:35 PM
You want to set both ARR and CCRx being preloaded. Read the RM. Maybe Cube does this fit you, I don't know, I don't use Cube
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.