STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32F103 uart2 Tx dma transmission doesn't Works corretly

I am using the stm32f103 and trying to display a text on a screen via DMA to the USART 2 device. I guess I will turn on the usart2 TX dma (DMAT) request when I need it and turn it off after the current transmission is complete (i.e. in the DMA1_Chann...

Positive Feedback: Resources now also list datasheet!

as I proposed some time ago, now products->Mikrocontrollers->Resources lists also datasheets. That way, one does not have to check the individual product pages for datasheet updates.Some other proposal however is still pending:List the documents newe...

Where can i find source code/examples for STWBC uC?

I've searched through the internet but i'm not able to find any firmware or source for coding the STWBC, atleast a few examples on how to do it. STM provides a binary as firmware to download and use it directly on the evaluation board. But i want to ...

SShow.1 by Associate II
  • 1311 Views
  • 1 replies
  • 0 kudos

Problems with timers and LEDS in NUCLEO G031K8

I'm having a problem where I'm controlling 9 LEDs with timers. Whenever I enter stand-by mode, the LEDs turn on/stay on. I want them to turn off. I can shut them down before stand-by mode but as I enter, they turn on. I've tried switching timers in...

0693W000001cZusQAE.png 0693W000001cZunQAE.png
varo1111 by Associate II
  • 1036 Views
  • 1 replies
  • 0 kudos

STM32F4 SPI Slave problems (wrong transmission)

Hello,I'm struggling to get the SPI Slave on my STM32F4 running. I send 9 Byte from the master every 1ms with soft NSS: HAL_GPIO_WritePin( MCU_CS_GPIO_Port, MCU_CS_Pin, GPIO_PIN_RESET ); SPISlaveTXdata[0] = frameCounter++; SPISlaveTXdata[1] = sys_g...

0693W000001cYd2QAE.png 0693W000001cYeAQAU.png
KR51K by Associate III
  • 1242 Views
  • 2 replies
  • 0 kudos

STM32F303C8 with using ADC1, ADC2

hey guys,​i'm programming a two motor control system, and must take each of motor current information. (my MCU's ADC setting : DMA, TRGO.)​when i get ADC's value using hal libraries, how can i get each of ADC1, ADC2 value???​In simple terms : I want...

HLee.6 by Associate
  • 1477 Views
  • 3 replies
  • 0 kudos

How can I count external PWM pulses with STM32F072?

Hello, I'm developing a custom board based on STM32F072B-DISCOVERY board.I have an external PWM source with variable frequency (from 200Hz to 10Khz), i need to count how many pulses it generates. How can it be done? PS. I've tried with Imput Compare ...

AComa.170 by Associate II
  • 1588 Views
  • 2 replies
  • 0 kudos

Hi , I am working on STM32f103zf , trying to get UART2 and UART3 to work with no success, UART1 is working ok. When I try to init UART2 I see that the the CR1 register is not being written although driver is trying to write to it and enable the UART.

The CR1 register stays 0 (as well as CR2, it looks like all UART2 registers are 0). My first thought was that the Bus is not enabled - as UART1 is on APB2 and UART 2 and 3 are on APB1 , but I enable UART2 bus - this is the enable code :   /* Enable G...

ASega by Associate II
  • 1783 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.