STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using interrupts (too quickly) prevents PWM from working?

I fixed my mistakes from my last iteration of code (reduced 6MHz interrupt rate (which is impossible) to around 35KHz,) and reduced the amount of code in the interrupt. PWM on any timer still refuses to work even though I've enabled them. Is it possi...

JShel.1 by Associate II
  • 1352 Views
  • 1 replies
  • 0 kudos

STM32H7 IWDG is not disabled after software reset.

My application requires to be started without watchdog enabled (don't ask why). But it seems that once enabled, after a software reset the IWDG continues to run, and if not treated in time causes to another reset. Note that the "Hardware watchdog�? ...

mmari.14 by Associate
  • 795 Views
  • 0 replies
  • 0 kudos

STM32 ADC power supply

Customer asks me to use STM32 powered from 3.3V with ADC reference 3.3V too (different source). So there is two possibel topologies:Connect VDD and VDDA, use precision source for VREFConnect VDDA and VREF to precision source, VDD connect to standard ...

LSind.1 by Associate
  • 1329 Views
  • 1 replies
  • 0 kudos

How to use 1 channel encoder on STM32F103?

Hello, I'm using STM32F103 on CUBE MX, when I used an encoder which has only 1 channel, nothing was added to encoder register. I get data from this function: __HAL_TIM_GET_COUNTER(&htim3). So does it has any different when we config encoder mode with...

Export restrictions on STM32 MCUs?

I ordered a bunch of STM32L443CCU6 chips from element14. I got an email from them saying that there are export restrictions on the chips. I’m based in India. How do I get these chips now?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.