STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32F407, stm32F072 and CAN bus

hello, i am trying to connect a stm32F407 and stm32F072 via CAN bus. but i cnt manage to get it done. i successfully connected two F407 via CAN bus and i used the same code for both of the boards . both of them transmitt the data perfectally but none...

SGUIG.1 by Associate II
  • 1279 Views
  • 0 replies
  • 0 kudos

N-pulse waveform generation application example - part2 (AN4776)

Hi .I have problem with this back to back timer configuration . (in AN4776)What I get :1- Timer 1 is making PWM ( i just need a regular pwm but this examle is a complementary one )2-Timer 1 will send a trigger to timer2( which is it's controller acut...

0693W000001pLJoQAM.png
M N by Associate II
  • 2385 Views
  • 6 replies
  • 0 kudos

STM32G474 ADC Master-Slave

I am slightly confused with the ADC Master - Slave configuration. Maybe someone can shed a bit of light in here.Using a STM32G474RET (LQFP64), thinking of chaining ADC1 and 2 in a master/slave configuration. Looking at the attached schematic, PB1 and...

Resolved! STM32F446 synced timers with phase shift

Hello,I'm using a Nucleo F446ZE to test timer capabilities to make a peak-and-hold PWM driver. I already have the core functionality where TIM1 uses DMA to run through a buffer of variable duty cycles at a higher frequency (e.g. 5 kHz) for the high-s...

0693W000001pLB1QAM.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.