2020-05-19 8:13 AM
I am slightly confused with the ADC Master - Slave configuration. Maybe someone can shed a bit of light in here.
Using a STM32G474RET (LQFP64), thinking of chaining ADC1 and 2 in a master/slave configuration. Looking at the attached schematic, PB1 and PB2 in such a configuration, what would they be named in such an ADC setup ?
Thanks,
Manu
2020-05-20 11:46 AM
Replying to my own question, after an extensive search:
I find that PB1 and PB2 are unusable simultaneously, as they both share IN12 ?
Can someone confirm this ?
Another question that I have on the same topic:
ADC1 & 2 used in Master - Slave mode (Dual Regular Simultaneous: LL_ADC_MULTI_DUAL_REG_SIMULT)
In this case can DMA1 Channel1 be used to service ADC12 Master Slave as a combo ADC, rather than having 2 DMA channels ?
I was thinking of something like this:
/* Set DMA transfer addresses of source and destination */
LL_DMA_ConfigAddresses(DMA1,
LL_DMA_CHANNEL_1,
LL_ADC_DMA_GetRegAddr(ADC1, LL_ADC_DMA_REG_REGULAR_DATA_MULTI),
(uint32_t)&adc_buf,
LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
Can that work ?
There appears to be a lot of silence on the forum ..
Can someone please help ?
Thanks,
Manu
2020-05-25 10:17 AM
You can do what you are thinking - use ADC1_IN12 on PB1 and ADC2_IN12 on PB2.
The pin naming scheme is:
Function | Instance | Channel
So, these are separate connections to different ADCs.
An example of a shared pin is: ADC12_IN14 on PB11.
Figure 84 to 88 in RM0440, Rev 4 are a handy reference.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.