2020-05-31 5:40 PM
Hi, i'm using my STM32F7 nucleo 144 and i'm learning about timer encoder mode and i follow the example in the datasheet but when i check the CNT register it oscillates in the same values and if i use the A0-A1 pins the encoder works bad, can somebody help me please?
// ******************* PORT ****************
RCC->AHB1ENR |=0x03; // Turn on A,B clocks
// *******************************************
// ******************* PINS *****************
GPIOA->MODER |=0x800; // Alternative A5
GPIOA->AFR[0] =0x100000; // Alternative function AF1
GPIOB->MODER |=0x80; // Alternative B3
GPIOB->AFR[0] =0x1000; // Alternative Function AF1
// *******************************************
// ******************* ENCODER TIMER********
RCC->APB1ENR |=0x01; // Turn on the TIM2 clock
TIM2->ARR =1000; // Maximun count
TIM2->CCMR1 |=0x0101; // select TI1 and TI2
TIM2->SMCR |=0x03; // Encoder mode 3
TIM2->CR1 |=0x01; // Timer On
// *******************************************
2020-05-31 5:54 PM
Which 'F7?
Read out and check the GPIO registers content, in debugger. In debugger, observe the given pins' GPIO_IDR bit, if it changes according to the input signal. Check (using the Nucleo's User manual), if on the board there's nothing connected to given pins.
> if i use the A0-A1 pins the encoder works bad,
Do you mean PA0 and PA1? What exactly do you mean by "works bad"?
JW
2020-05-31 6:09 PM
I use the STM32F746ZGTX, and i check the GPIOA->IDR register in the debugger like you told me and it is strange, if i don't touch the encoder the PA1 pin oscillates. i wrote that works bad and exactly is that, when i move the encoder, for example 1 step in the debugger the cnt change 3 steps or 2 steps
2020-05-31 6:15 PM
> if i don't touch the encoder the PA1 pin oscillates.
Yes, but that's really what's happening on the encoder's output, isn't it.
Use an oscilloscope to observe the encoder's behaviour.
> 1 step in the debugger the cnt change 3 steps or 2 steps
1 step of what? You mean 1 detent on encoder intended as manual input? Those tend to produce a full four-quadrant signal upon moving one detent, so setting timer to count on both edges, it may quite well be that each detent increments the counter by 4.
JW
2020-06-03 12:06 PM
Thanks, when i conected my osciloscope i watched the proble, it was the cable between my encoder and the stm. if i move the encoder, the stm recognize it and the direction is correct. most all was perfect the "problem" is the value of the CNT register. I move my rotative encoder 1 step (my encoder is the 20 steps) but the CNT count 4 steps or 3 steps. i putted diferents values of the filter, the prescaler but always the CNT count the same values (3 steps or 4 if i move just 1 step in my encoder)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.