STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401 plus VL53L1X crashes after 10 mins

Hi Guys,I'm using an STM32F401 board, accompanied an expansion board, and by a VL53L1X (people counter) sensor. It works for 10minutes then the board crashes and the only way to get it working again is by resetting the board.Hi Guys, What I'm usingST...

AElek.1 by Associate
  • 1078 Views
  • 0 replies
  • 0 kudos

stm32l010 analog watchdog

Can the analog watchdog work with oversampling? If so, will it monitor only the converted values after a full oversampling cycle?

adaniel by Associate III
  • 1279 Views
  • 2 replies
  • 0 kudos

unexpected reset after changing the GPIO mode on Fly.

Dear experts, my STM32F042G6 is unexpectedly reset after I switched on fly CAN_TX GPIO to output GPIO pin.  for this I did this steps.1).HAL_CAN_STOP() and then  2). GPIOA->MODER &= ~((U32) "pinX");   GPIOA->MODER|= ~(U32) "pinX");I have also made th...

RHeza.1 by Associate
  • 1393 Views
  • 2 replies
  • 0 kudos

Cannot use SPI TSIZE in Simplex receive only mode on STM32H7 ?

A question about this sentence of STM32H7 reference manual:Receive-only mode: COMM[1:0]=10In master mode, the MOSI output is disabled and may be used as GPIO. The clocksignal is generated continuously as long as the SPI is enabled and the CSTART bit ...

Gpeti by Senior II
  • 742 Views
  • 0 replies
  • 0 kudos

Differences between PWM channels 2, 3, 4 in TIM8?

I think I am missing something obvious about a difference between channels 2&3 vs channel 4 in the TIM8 after staring at this for some hours now...I am using the STM32H750 discovery board, and created a project in CubeMX which configures PI2, PB14 an...

0693W000001pty7QAA.png 0693W000001ptyMQAQ.png 0693W000001ptyHQAQ.png 0693W000001pty8QAA.png
KJ.2 by Associate
  • 2432 Views
  • 3 replies
  • 3 kudos

Software download issue

Software download issueHi, I have met the same issue like this. Should I also wait an hour until this package been prepared?

Lhong.1 by Associate II
  • 1370 Views
  • 3 replies
  • 0 kudos

Can the SPI run at another voltage apart from VDD?

The data sheet isn't specific, apart from one diagram Figure 13 that shows IO's box with an arrow from VDD that then connects to a level shifter to the core domain.Please advise. A real handy feature would be to alternative voltage IO for the SPI's...

MMars.1 by Associate
  • 1687 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.