STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U575 System Bootloader SPI MISO issue

I am evaluating using SPI and ST's internal System Bootloader for a 2 processor application.To that end, I am attempting to attempt to read in the bootloader via SPI on an STLink V3.I am successfully able to do so for a NUCLEO-L496ZG, but fails for a...

DS1Z_QuickPrint78.png

i2s_ckin vs. PLLI2S

Hi,I'm using an STM32C051K6T6 to read an audio file from FLASH (a book on tape, basically) and output the data over I2S to a codec/amplifier. I would like to understand the drawbacks, if any, of using the internally generated PLLI2SCLK instead of an ...

how to interface 50 pin lvds 1920*720 in f769-dis0

Hi ST-Members,I need to interface a 10.3-inch LVDS display with a resolution of 1920x720 to an STM32F769-disc0. I also have an H743 Nucleo board. Could you please advise on the method I should use to make the display work? Additionally, I plan to ini...

DS90C385AMT.png
mbed_engr by Associate II
  • 3074 Views
  • 1 replies
  • 0 kudos

Resolved! SPI communication using DMA on the STM32H743.

SPI communication using DMA on the STM32H743.We have created a program for SPI communication using DMA, The first send/receive with HAL_SPI_TransmitReceive_DMA is successful.However, when the exact same process is executed afterwards, all received va...

Resolved! UART IRQ fired but no IRQ source configured

Hello,I have a H7 design with multiple UART/USART used to communicate via RS485 drivers (XR3072).I have programmed kind of loopback test by connecting the A/B signals of two RS485 busses.For this I use 2 DMA channels for each UART, one for RX and one...

uart_irq_status.png
regjoe by Senior II
  • 2567 Views
  • 9 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.