STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer registers to be updated simultaneously

Hi,I am using STM32G474 with TIM1, TIM8 and TIM20 and working with STM32CubeIDE.I want to updatethe ARR, CCR1, CCR2 and CCR3 regs at the same time. I taught that with the preload register it can be done but it doesn't work for me.So how can I do to s...

DKuro.1 by Associate III
  • 1521 Views
  • 3 replies
  • 0 kudos

F429 - DMA - Memory to Peripheral Broken!

Hi All,I am having trouble with DMA transfers using a F429.I am using DMA1, Channel2, Stream6 - regulated by TIM4 Updates.It is a memory to perpheral, 32 bit, single transfer, double buffer Off - from Flash (AHB3) to GPIOG (AHB1).However, it breaks o...

PSPF by Associate II
  • 3679 Views
  • 8 replies
  • 0 kudos

QSPI peripheral state remains busy when using DMA

Hi,I'm trying to use QSPI to interface with a flash memory chip (GD25Q16). I can read and write to memory and status registers using blocking code, but I'd like to use DMA to decrease the CPU load. However, the QSPI handle's State gets stuck in HAL_Q...

BBagl.1 by Associate
  • 1969 Views
  • 2 replies
  • 0 kudos

STM32L011 + systick + WFI problem

Hello, my STM32L011's core is running at 32 MHz. I use systick for 1 ms interrupt. However, if i try to use the WFI inside my while loop in my delay function, the timebase changes from 1 ms to 6.28 ms. Any help is appreciated!#include "user_systick.h...

LBogd.2 by Associate II
  • 2591 Views
  • 5 replies
  • 0 kudos

Resolved! In STM32F7508-DK board , If all flash of 64 KB is occupied, Can we use QSPI Flash ? If yes then what is exact procedure ? Is there any drawback ?

We are Planning to Use STM32F7508-DK board for our Application. As I go through Datasheet of it. It is mention that 64 KB for internal flash. But I am very sure that my application required more than 64 KB. Question : Can we use QSPI Flash in case ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.