2020-08-06 5:36 PM
Hi All,
I am having trouble with DMA transfers using a F429.
I am using DMA1, Channel2, Stream6 - regulated by TIM4 Updates.
It is a memory to perpheral, 32 bit, single transfer, double buffer Off - from Flash (AHB3) to GPIOG (AHB1).
However, it breaks on the first attempted transfer with setting TEIF6 in the DMA_HISR register - I have NO idea why!
According to the data sheet I am doing everything right.
Can anyone tell me why?
Thanks
PSPF
2020-08-06 5:48 PM
I bet if you showed your code, someone could spot the bug. The reference manual lists a number of conditions that will trigger TEIF. You're likely causing one of those.
2020-08-06 6:18 PM
Thank you for your reply TDK.
I am using STM32CubeIDE. Not shown in the code below, but I have setup break points so I could examine the the registers;-
DMA CR = 0x04025540
DMA PAR = 0x40021818
DMA M0AR = 0x08004D0C
DMA NDTR = 3
DMA FCR = 0x20
....
#define TryDMA_Pin GPIO_PIN_0
#define TryDMA_GPIO_Port GPIOG
static const uint32_t GPO[] = {TryDMA_Pin, TryDMA_Pin << 16,
TryDMA_Pin, TryDMA_Pin << 16,
TryDMA_Pin, TryDMA_Pin << 16,
TryDMA_Pin, TryDMA_Pin << 16};
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_TIM4_Init();
HAL_DMA_Start(&hdma_tim4_up, (uint32_t)RAMTab, (uint32_t)&TryDMA_GPIO_Port->BSRR, 4);
htim4.Instance->DIER |= TIM_DIER_UDE;
HAL_TIM_OC_Start(&htim4, TIM_CHANNEL_2);
while (1)
{
}
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Stream6_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream6_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream6_IRQn);
}
static void MX_TIM4_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_SlaveConfigTypeDef sSlaveConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
htim4.Instance = TIM4;
htim4.Init.Prescaler = 84;
htim4.Init.CounterMode = TIM_COUNTERMODE_DOWN;
htim4.Init.Period = 1023;
htim4.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim4.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim4) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim4, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OC_Init(&htim4) != HAL_OK)
{
Error_Handler();
}
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_GATED;
sSlaveConfig.InputTrigger = TIM_TS_TI1FP1;
sSlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_BOTHEDGE;
sSlaveConfig.TriggerFilter = 0;
if (HAL_TIM_SlaveConfigSynchro(&htim4, &sSlaveConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC2REF;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim4, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_TOGGLE;
sConfigOC.Pulse = 511;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_OC_ConfigChannel(&htim4, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
HAL_TIM_MspPostInit(&htim4);
}
2020-08-07 2:47 AM
In F4, you can't use DMA1 to transfer to GPIO. Use DMA2 (thus TIM1 or TIM8 to trigger the DMA).
JW
2020-08-07 10:15 AM
Are you sure you can transfer data from "Flash memory" using DMA? As I know the flash memory region have special read procedure. usually DMA is used to transfer data from/to RAM memory space.
2020-08-07 2:10 PM
> Are you sure you can transfer data from "Flash memory" using DMA?
Yes.
See RM0090, Fig.2. Both DMA connect as masters to the slave bus, which goes to the FLASH controller's data port (the same bus to which processor's D-port connects, too).
Of course, it has the respective impact on latencies (i.e. at higher system clocks the FLASH waitstates apply) and interacts with the data cache in ART, exactly in the same way as processors data access through the D-port.
JW
2020-08-07 2:38 PM
That's a MEMORY to MEMORY transfer, not MEMORY to/from APB1, you need DMA2, it has better plumbing..
2020-08-09 5:03 PM
Thank you everyone for your help.
I will move it to DMA2, and give it a go.
I must admit, I didn't see figure 2 - I did get confused trying to unravel the spiderweb of figure 34...
I will post here the results - hopefully later today.
Thanks again
PSPF
2020-08-10 7:23 PM
Thanks everyone - changing it from DMA1 to DMA2 and using TIM8 fixed it...!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.