2020-08-07 6:56 AM
Hey Guys, iam trying to convert Arduino Code to my C Project in CubeIDE..
I have some troubles(=warnings and iam unsure) with the SPI Trasmit functions.
Could you tell me if my code does the same as the Arduino Code?
ARDUINO :
*******************
void SX126XLT::readRegisters(uint16_t address, uint8_t *buffer, uint16_t size)
{
#ifdef SX126XDEBUG
//Serial.println(F("readRegisters()"));
#endif
uint16_t index;
uint8_t addr_l, addr_h;
addr_h = address >> 8;
addr_l = address & 0x00FF;
checkBusy();
#ifdef USE_SPI_TRANSACTION //to use SPI_TRANSACTION enable define at beginning of CPP file
SPI.beginTransaction(SPISettings(LTspeedMaximum, LTdataOrder, LTdataMode));
#endif
digitalWrite(_NSS, LOW);
SPI.transfer(RADIO_READ_REGISTER);
SPI.transfer(addr_h); //MSB
SPI.transfer(addr_l); //LSB
SPI.transfer(0xFF);
for (index = 0; index < size; index++)
{
*(buffer + index) = SPI.transfer(0xFF);
}
digitalWrite(_NSS, HIGH);
#ifdef USE_SPI_TRANSACTION
SPI.endTransaction();
#endif
}
void SX126XLT::writeRegisters(uint16_t address, uint8_t *buffer, uint16_t size)
{
#ifdef SX126XDEBUG
//Serial.println(F("writeRegisters()"));
#endif
uint8_t addr_l, addr_h;
uint8_t i;
addr_l = address & 0xff;
addr_h = address >> 8;
checkBusy();
#ifdef USE_SPI_TRANSACTION //to use SPI_TRANSACTION enable define at beginning of CPP file
SPI.beginTransaction(SPISettings(LTspeedMaximum, LTdataOrder, LTdataMode));
#endif
digitalWrite(_NSS, LOW);
SPI.transfer(RADIO_WRITE_REGISTER);
SPI.transfer(addr_h); //MSB
SPI.transfer(addr_l); //LSB
for (i = 0; i < size; i++)
{
SPI.transfer(buffer[i]);
}
digitalWrite(_NSS, HIGH);
#ifdef USE_SPI_TRANSACTION
SPI.endTransaction();
#endif
}
***************
c in CubeIDE :
***************
void readRegisters(uint16_t address, uint8_t *buffer, uint16_t size)
{
#ifdef SX126XDEBUG
uint8_t s[] ="readRegisters() \r\n";
tx_com(s, strlen((char const*)s));
#endif
uint16_t index;
uint8_t addr_l, addr_h;
addr_h = address >> 8;
addr_l = address & 0x00FF;
checkBusy();
HAL_GPIO_WritePin(SX1261_NSS_GPIO_Port, SX1261_NSS_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, RADIO_READ_REGISTER, sizeof(RADIO_READ_REGISTER), HAL_MAX_DELAY);
HAL_SPI_Transmit(&hspi1, addr_h, sizeof(addr_h), HAL_MAX_DELAY);
HAL_SPI_Transmit(&hspi1, addr_l, sizeof(addr_l), HAL_MAX_DELAY);
HAL_SPI_Transmit(&hspi1, 0xFF, sizeof(0xFF), HAL_MAX_DELAY);
HAL_SPI_TransmitReceive(&hspi1, 0xFF, buffer, size, HAL_MAX_DELAY);
HAL_GPIO_WritePin(SX1261_NSS_GPIO_Port, SX1261_NSS_Pin, GPIO_PIN_SET);
}
void writeRegisters(uint16_t address, uint8_t *buffer, uint16_t size){
#ifdef SX126XDEBUG
uint8_t s[] ="writeRegisters() \r\n";
tx_com(s, strlen((char const*)s));
#endif
uint8_t addr_l, addr_h;
addr_l = address & 0xff;
addr_h = address >> 8;
checkBusy();
HAL_SPI_Transmit(&hspi1, RADIO_WRITE_REGISTER, sizeof(RADIO_WRITE_REGISTER), HAL_MAX_DELAY);
HAL_SPI_Transmit(&hspi1, addr_h, sizeof(addr_h), HAL_MAX_DELAY); //MSB
HAL_SPI_Transmit(&hspi1, addr_l, sizeof(addr_l), HAL_MAX_DELAY); //LSB
HAL_SPI_Transmit(&hspi1, buffer, size, HAL_MAX_DELAY);
HAL_GPIO_WritePin(SX1261_NSS_GPIO_Port, SX1261_NSS_Pin, GPIO_PIN_SET);
}I dont know if iam using the right functions and if i have the right arguments .
Esspecially the 2nd Argument in the HAL_SPI_Transmit(); function ..
CubeIDE gives me a warning : makes pointer from integer without a cast [-Wint-conversion]
thank you
2020-08-07 9:27 AM
you should use & operator to convert uint8_t to uint8_t* (a pointer). like this:
HAL_SPI_Transmit(&hspi1, &addr_h, sizeof(addr_h), HAL_MAX_DELAY);
2020-08-07 11:14 PM
alright, thank you very much. That makes sence to me because the HAL Manual says : HAL_StatusTypeDef HAL_SPI_Transmit (SPI_HandleTypeDef * hspi, uint8_t * pData, uint16_t Size, uint32_t Timeout)
next question:
The Arduino Codes sends byte by byte in a loop :
SPI.transfer(addr_h); //MSB
SPI.transfer(addr_l); //LSB
for (i = 0; i < size; i++)
{
SPI.transfer(buffer[i]);
}is is correct to replace that with one HAL_SPI_Transmit method?
HAL_SPI_Transmit(&hspi1, &addr_h, sizeof(addr_h), HAL_MAX_DELAY); //MSB
HAL_SPI_Transmit(&hspi1, &addr_l, sizeof(addr_l), HAL_MAX_DELAY); //LSB
HAL_SPI_Transmit(&hspi1, &buffer, size, HAL_MAX_DELAY);annother question:
&addr_h is a pointer to an adress. HAL_SPI_Transmit needs the number of bytes to transmit in the 3rd argument. Is it correct to say sizeof(addr-h) ? i guess not..
is it sizeof(&addr_h) ? or should i just say the length is 4 because the adress stores 32bit? am i thinking right?
2020-08-08 3:35 AM
1- yes, you can send multiple bytes at once.
2- sizeof(addr_h) is correct. sizeof will return number of bytes that the input variable occupied.
2020-08-09 11:18 PM
got it!
what about the following:
void readCommand(uint8_t Opcode, uint8_t *buffer, uint16_t size){
[...]
HAL_SPI_Transmit(&hspi1, &Opcode, sizeof(Opcode), HAL_MAX_DELAY);
HAL_SPI_Transmit(&hspi1, 0xFF, sizeof(0xFF), HAL_MAX_DELAY);
HAL_SPI_TransmitReceive(&hspi1, 0xFF, buffer, size, HAL_MAX_DELAY); }line 4 and 5 are giving me the warning: passing argument 2 of 'HAL_SPI_Transmit' makes pointer from integer without a cast [-Wint-conversion]
The Argument 0xFF istn stored anywhere, so i cant create a pointer pointing to it, right?
i translated that from :
void SX126XLT::readCommand(uint8_t Opcode, uint8_t *buffer, uint16_t size){ [...]
SPI.transfer(Opcode);
SPI.transfer(0xFF);
for ( i = 0; i < size; i++ ){
*(buffer + i) = SPI.transfer(0xFF);
}
}i just wanna make sure that my code is doint the same thing as the arduino code
thank you guys, iam learning a lot here;)
2020-08-09 11:36 PM
You can put 0xFF in an array like
uint8_t tx_buffer[] = { 0xFF };
HAL_SPI_Transmit(&hspi1, tx_buffer, sizeof(tx_buffer), HAL_MAX_DELAY);
2020-08-10 2:26 AM
why would you suggest an array and not a simple variable? would that be a pointer then?
2020-08-10 2:41 AM
You can use a simple variable as well. There is barely any difference but the array is more generic as in
uint8_t tx_buffer[] = { 0xFF, 0xAA, 0x55 };
HAL_SPI_Transmit(&hspi1, tx_buffer, sizeof(tx_buffer), HAL_MAX_DELAY);and similiarily for rx_buffer of known length.
> would that be a pointer then?
Arrays decay to pointers in C automatically, i.e. tx_buffer can be used instead of &tx_buffer[0].
2020-08-10 4:39 AM
that makes sence! thanks
void startWriteSXBuffer(uint8_t ptr) {
[...]
HAL_SPI_Transmit(&hspi1, ??ptr, sizeof(ptr), HAL_MAX_DELAY);
}
how i can solve this ? HAL_SPI_Transmit needs a pointer in the 2nd Argument.
Should i create a pointer variable?
2020-08-10 5:00 AM
You should learn more about C.
void startWriteSXBuffer(uint8_t *ptr, uint16_t size) {
[...]
HAL_SPI_Transmit(&hspi1, ptr, size, HAL_MAX_DELAY);
}
C pointers are dumb and don't know the size of the thing they are pointing at.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.