2020-09-01 10:02 PM
Hi,
I wanted to Erase and write data to select Flash memory location.
I have Nucleo-L4R5ZI kit and have example Flash erase code available for L4 series which I ported to R5ZI.
As you can see, the example code has two portions:
Problem am facing is this:
I want to erase page 16 i.e starting address is 0x08010000
So I am using EraseInitStruct where I feed what type to erase, which page to erase and which bank the page belongs to, all these data.
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Banks = 1;
EraseInitStruct.Page = 0x10;
EraseInitStruct.NbPages = 1;
Problem is, instead of erasing only the page 16, it erases 17,18,19 along with 16. Am using 2 bank configuration. So a page has 4096 bytes (4KB). For my code, page starting from 0x08010000 and ending at 0x08010fff should have been erased. But it erases till 0x08013fff.
What am I missing ? Herewith attaching the source file for your reference.
/**
******************************************************************************
* @file FLASH/FLASH_EraseProgram/Src/main.c
* @author MCD Application Team
* @brief This example provides a description of how to erase and program the
* STM32L4xx FLASH.
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2017 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/** @addtogroup STM32L4xx_HAL_Examples
* @{
*/
/** @addtogroup FLASH_EraseProgram
* @{
*/
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
#define FLASH_USER_START_ADDR ADDR_FLASH_PAGE_16 /* Start @ of user Flash area */
#define FLASH_USER_END_ADDR ADDR_FLASH_PAGE_255 + FLASH_PAGE_SIZE - 1 /* End @ of user Flash area */
#define DATA_64 ((uint64_t)0x1234567812345678)
#define DATA_32 ((uint32_t)0x12345678)
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
uint32_t FirstPage = 0, NbOfPages = 0, BankNumber = 0;
uint32_t Address = 0, PAGEError = 0;
__IO uint32_t data32 = 0 , MemoryProgramStatus = 0;
/*Variable used for Erase procedure*/
static FLASH_EraseInitTypeDef EraseInitStruct;
/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);
static uint32_t GetPage(uint32_t Address);
static uint32_t GetBank(uint32_t Address);
/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program
* @param None
* @retval None
*/
int main(void)
{
/* STM32L4xx HAL library initialization:
- Configure the Flash prefetch
- Systick timer is configured by default as source of time base, but user
can eventually implement his proper time base source (a general purpose
timer for example or other time source), keeping in mind that Time base
duration should be kept 1ms since PPP_TIMEOUT_VALUEs are defined and
handled in milliseconds basis.
- Set NVIC Group Priority to 4
- Low Level Initialization
*/
HAL_Init();
/* Configure the system clock to 120 MHz */
SystemClock_Config();
/* Initialize LED1, LED2 and LED3 */
BSP_LED_Init(LED1);
BSP_LED_Init(LED2);
BSP_LED_Init(LED3);
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
/* Erase the user Flash area
(area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/
/* Clear OPTVERR bit set on virgin samples */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
/* Get the 1st page to erase */
FirstPage = GetPage(FLASH_USER_START_ADDR);
/* Get the number of pages to erase from 1st page */
NbOfPages = GetPage(FLASH_USER_END_ADDR) - FirstPage + 1;
/* Get the bank */
BankNumber = GetBank(FLASH_USER_START_ADDR);
/* Fill EraseInit structure*/
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Banks = BankNumber;
EraseInitStruct.Page = FirstPage;
EraseInitStruct.NbPages = NbOfPages;
/* Note: If an erase operation in Flash memory also concerns data in the data or instruction cache,
you have to make sure that these data are rewritten before they are accessed during code
execution. If this cannot be done safely, it is recommended to flush the caches by setting the
DCRST and ICRST bits in the FLASH_CR register. */
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGEError) != HAL_OK)
{
/*
Error occurred while page erase.
User can add here some code to deal with this error.
PAGEError will contain the faulty page and then to know the code error on this page,
user can call function 'HAL_FLASH_GetError()'
*/
/* Infinite loop */
while (1)
{
BSP_LED_On(LED3);
}
}
/* Program the user Flash area word by word
(area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/
Address = FLASH_USER_START_ADDR;
while (Address < FLASH_USER_END_ADDR)
{
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Address, DATA_64) == HAL_OK)
{
Address = Address + 8;
}
else
{
/* Error occurred while writing data in Flash memory.
User can add here some code to deal with this error */
while (1)
{
BSP_LED_On(LED3);
}
}
}
/* Lock the Flash to disable the flash control register access (recommended
to protect the FLASH memory against possible unwanted operation) *********/
HAL_FLASH_Lock();
/* Check if the programmed data is OK
MemoryProgramStatus = 0: data programmed correctly
MemoryProgramStatus != 0: number of words not programmed correctly ******/
Address = FLASH_USER_START_ADDR;
MemoryProgramStatus = 0x0;
while (Address < FLASH_USER_END_ADDR)
{
data32 = *(__IO uint32_t *)Address;
if (data32 != DATA_32)
{
MemoryProgramStatus++;
}
Address = Address + 4;
}
/*Check if there is an issue to program data*/
if (MemoryProgramStatus == 0)
{
/* No error detected. Switch on LED1*/
BSP_LED_On(LED1);
}
else
{
/* Error detected. Switch on LED2*/
BSP_LED_On(LED2);
}
/* Infinite loop */
while (1)
{
}
}
/**
* @brief Gets the page of a given address
* @param Addr: Address of the FLASH Memory
* @retval The page of a given address
*/
static uint32_t GetPage(uint32_t Addr)
{
uint32_t page = 0;
if (Addr < (FLASH_BASE + FLASH_BANK_SIZE))
{
/* Bank 1 */
page = (Addr - FLASH_BASE) / FLASH_PAGE_SIZE;
}
else
{
/* Bank 2 */
page = (Addr - (FLASH_BASE + FLASH_BANK_SIZE)) / FLASH_PAGE_SIZE;
}
return page;
}
/**
* @brief Gets the bank of a given address
* @param Addr: Address of the FLASH Memory
* @retval The bank of a given address
*/
static uint32_t GetBank(uint32_t Addr)
{
uint32_t bank = 0;
if (READ_BIT(SYSCFG->MEMRMP, SYSCFG_MEMRMP_FB_MODE) == 0)
{
/* No Bank swap */
if (Addr < (FLASH_BASE + FLASH_BANK_SIZE))
{
bank = FLASH_BANK_1;
}
else
{
bank = FLASH_BANK_2;
}
}
else
{
/* Bank swap */
if (Addr < (FLASH_BASE + FLASH_BANK_SIZE))
{
bank = FLASH_BANK_2;
}
else
{
bank = FLASH_BANK_1;
}
}
return bank;
}
Regards,
Karthik
2020-09-08 9:51 AM
Hello Karthik,
Replace
#define FLASH_USER_END_ADDR ADDR_FLASH_PAGE_255 + FLASH_PAGE_SIZE - 1 /* End @ of user Flash area */with
#define FLASH_USER_END_ADDR ADDR_FLASH_PAGE_16 + FLASH_PAGE_SIZE - 1 /* End @ of user Flash area */and only page 16 will be erased.
Br,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.