STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-F030R8, Virtual Com Port

Purpose: try to print "hello world" .Status: VCP shown in Device Manager as COM3. Putty can connect. Nothing displayed, tried other serial port debug tool. No success. simple code, except HAL_UART_Transmit, all others are auto-generated by CubeIDE. U...

YLu.1 by Associate
  • 1168 Views
  • 1 replies
  • 0 kudos

PWM on STM32l4 stops working randomly

I have a problem that the PWM timer stops working randomly, maybe once every 2 weeks on 4 prototoypes. The PWM signal is just high instead of the frequency it should do. I have added reset and recover but nothing seems to fix. Since I am not able to ...

rickard2 by Associate III
  • 3566 Views
  • 7 replies
  • 0 kudos

STM32F4 Timer interrupt and Sending data over Usart

I am using the STM32F407VET6 and SPL libraries. My goal is very straightforward, just send data over usart periodically.But when I send data (buttoncheck function) inside the timer interrupt it stucks " while(USART_GetFlagStatus(USART3, USART_FLAG_TC...

goktug by Associate
  • 1379 Views
  • 0 replies
  • 0 kudos

SPI Multi-master NSS Setup

HelloIm trying to implement stm32 spi multi-master function on a stm32f765 according to the below presentationI keep getting MODF error when transmitting as a master, that would indicate that the slave sets the masters NSS pin low. Even if I set the ...

0693W000003QsuWQAS.png

Resolved! Stop Transmit interrupt manually during transmitting

HiI'm doing a project to detect collision on UART, when I get data from Rx, I will compare it with the data I transmitted, if there aren't the same, means collision occurred, then I will immediately stop my transmitting interrupt to stop sources wast...

Olly Kao by Associate III
  • 2335 Views
  • 1 replies
  • 0 kudos

How to use DAC dual Channels simultaneously using DMA

Hello,I am using STM32F765BI MCU.I want to generate an audio on both the channel of DAC using DMA simultaneously, currently I am facing a problem that I am able to generate audio only on one DAC channel at a time.So please suggest a method that how c...

LDesa.1 by Associate II
  • 2682 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.