STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SMBUS/ PMBUS Expansion Package

I am trying to implement the PMBUS on STM32 processor using SMBUS/PMBUS exapnsion package. I am able to execute the read and write commands. But when I am trying to execute the READ_OR_WRITE command for read operation then I receive only FF FF in the...

NAgar.1 by Associate
  • 1472 Views
  • 1 replies
  • 0 kudos

why current consumption in low power sleep mode(LP SLEEP) on stm32G071RBT6 is around 1mA, not less than 100uA as spec?

I'm working on NUCLEO G071RB board to measure current consumption MCU STM32G071RBT6 in LP SLEEP mode. I run the example https://github.com/STMicroelectronics/STM32CubeG0/tree/be65d071640424445aa265e8b9a058e44b8decb7/Projects/NUCLEO-G071RB/Examples/PW...

DThan.1 by Associate
  • 1055 Views
  • 1 replies
  • 0 kudos

How to generate sinewave by using DAC in stm32h745xg ?

we are using stm32h745xg and I initialize DAC with timer 6 ,we enable DMA also.we are using following code  static TIM_HandleTypeDef htim; TIM_MasterConfigTypeDef sMasterConfig; /*##-1- Configure the TIM peripheral ##################################...

srikanth by Associate III
  • 840 Views
  • 0 replies
  • 0 kudos

Hi, I am completely new to STM32 MCU programming. I am trying to make a simple variable frequency complementary square wave generator with my STM32F103C8T6 blue pill to drive an inductive load. I'd like to use a potentiometer to vary the frequency.

Frequency range I'm looking for is from 60 kHz to 200 Khz. Here's the code I generated with Cube IDE. It initializes the GPIOs, ADC, and PWMs but I don't know how to integrate a potentiometer in this code and be able to vary the frequency of the comp...

SGulc.1 by Associate
  • 1374 Views
  • 1 replies
  • 0 kudos

TTCAN in STM32F767

Hello I have read on the reference manual that the CAN controller can be set to work as TTCAN by setting the TTCM bit. But comparing with the STM32H7 it seems that only the latter family has the TTCAN functionality.Someone has experience with that ?R...

DVicc.1 by Associate II
  • 1254 Views
  • 1 replies
  • 0 kudos

STM32F7 RTC Accuracy/Calibration Methods?

Hello Everyone, I am using the STM32F777 and utilizing its RTC and external 32.768 crystal(LSE).Currently I am having a drift of 79s in 76 hours. it is a little bit less than a second per hour. It is not that bad but I would like to have a better res...

Mauricio by Associate II
  • 1466 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.