2020-09-20 11:21 PM
Hello I have read on the reference manual that the CAN controller can be set to work as TTCAN by setting the TTCM bit. But comparing with the STM32H7 it seems that only the latter family has the TTCAN functionality.
Someone has experience with that ?
Regards
Dav
2020-09-21 4:13 AM
All non-FD CAN hardware has as an errata that TTCAN is not working. "BxCAN time triggered mode not supported"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.