2019-12-31 1:07 PM
I am trying to implement the PMBUS on STM32 processor using SMBUS/PMBUS exapnsion package. I am able to execute the read and write commands. But when I am trying to execute the READ_OR_WRITE command for read operation then I receive only FF FF in the output. Looking at the code, it says that if the command supports read then make the size = pStackContext->CurrentCommand->cmnd_master_Tx_Size, so even I just want to do a read operation for READ_OR_WRITE Command, it is expecting to receive the required data bytes specified in size.
Is there any work around to this problem?
Thanks
Nitish
2020-09-21 2:33 PM
Works for me like this in STACK_SMBUS_ExecuteCommand
uint8_t *piobuf = STACK_SMBUS_GetBuffer( pStackContext );
st_command_t *pCommand = pStackContext->CurrentCommand;
if (!piobuf || !pCommand) {
pStackContext->StateMachine |= SMBUS_SMS_ERROR;
return STACK_ERROR;
}
const bool is_write = ((pStackContext->StateMachine & SMBUS_SMS_RECEIVE) != SMBUS_SMS_RECEIVE) && ( ( pCommand->cmnd_query & WRITE ) == WRITE );
switch (pCommand->cmnd_code) {
case XXXX:
if (is_write)
set_XXXX(piobuf[0]);
piobuf[0] = get_XXXX();
return STACK_OK;
I am pretty sure there must be a better way to identify if it was a read or write operation than the above twisted condition.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.